AURIX™ Forum Discussions
hi,
使用I2C_Read_Ext_Device_1_KIT_TC397_TFT demo code 通过I2C 对EEROM(micochip 24AA02E48)进行写操作,device's internal address 设置为0x0000,可以写入8个byte的数据,但是写入第二笔的时候写不进去了,
请问,1.写完第一笔后device's internal address 需要设置为什么?
2.如何可以一次写入128byte的数据?(目前一次写入为8byte,多余8个byte 数据写不进去)
代码如下:
uint8 write_data[36];
uint16 addr = 0x0000;
// setup the device's internal address
write_data[0] = addr >> 8; // High byte
write_data[1] = (uint8)addr; // Low byte
// setup data to be written
write_data[2] = 0x01;
write_data[3] = 0x02;
write_data[4] = 0x03;
write_data[5] = 0x04;
write_data[6] = 0x05;
write_data[7] = 0x06;
write_data[8] = 0x07;
uint8 size = 9; // 5 bytes to transmit to i2cDev (data and internal address)
// write data to device as soon as it is ready
while(IfxI2c_I2c_write(&g_i2cDevEeprom, write_data, size) == IfxI2c_I2c_Status_nak);
请问infineon官方有没有对smu alarm的action的推荐配置?比如ALM0[0]推荐配成reset还是中断、fsp是否使能?
Hello,
I want to use an Aurix TC397 to send some images to another device using AVTP protocol. Where can I find some examples to help me?
Thank you!
Show LessHello,
How can I turn the lsl files of the programs in partitions A and B into one lsl file after enabling swap mode?
Or can we put the two programs in the AB partition into one project? If so, how can we implement it?
Best Regards,
Show LessHi, Community,
First time installing Bifacese on my PC.
After installing Bifacese, I started StartBifaces.bat in BifaceseWin64.
When I did so, I received the following error message
I assume this is due to a different Java PATH, but could you please tell me a workaround for this?
Best Regards,
Chihiro Tatebayashi / NEXTY
我正在使用TC39X芯片,並測試ASCLIN LIN master功能,並配合VECTOR CANOE做驗證。
使用'ASCLIN_LIN_Master_1_KIT_TC397_TFT' Example code,並將idle delay設置為0
LIN master 有成功丟出封包且封包格式卻符合邏輯 (error.jpg),但是CANOE報錯同步位元組錯誤,
請問是哪個部分設定有誤呢?
(有使用另一台LIN設備丟出同樣的封包但CANOE顯示封包正確,如correct.jpg)
謝謝
Show Lesshello.
We are currently conducting Ethernet testing using the Secrue Gateway-v1.1 board.
The Phy chip is using 88EA1512, but I cannot find the example source. Can you help with example source?
thank you
Hello Friends,
Could you help me please.
When starting the project, we configure the pin as output using davinci configurator after and during the execution of the software, I want to reconfigure the pin as input and read the state of the pin (HW configured in pull up), I am supposed to read 1.
the problem with the software below I cannot read the status of the pin, could you please help me by looking at what I have configured on the software?