AURIX™ Forum Discussions
Hi,
i need support to vary due cycle of PWM without varying frequency for every 10ms without glitches. Currently i am getting glitches which leads to unintended functionality of PWM to drive motor.
Thanks, and Regards
param
Show LessHi everyone,
It is possible to run the board without the debug mode in AURIX Develop Studio? My intention is to write the code in the flash and run without do the debug. Thank you in advance.
Show LessHi ,
I am using Ifx_Tc3xx_I2c package, the CPU is TC377, the I2C device needs a Read format as follows:
S,Slave Addr+0,Ack(slave), Regisger address, Ack, ReStart, Slave Addr+1, Data1,Ack, Data2,Ack,...,
In I2c.c in the folder, there are I2c_AyncWrite(), I2c_SyncWrite(), I2c_AyncRead(), I2c_SyncRead() APIs.
Could anyone show me how to generate the repeated start or provide the sample code.
Thanks
Show LessFor the TC367 processor, we use the P15.7 pin for LIN communication.
After we init LIN, when I send a wakeup request from the external world, RED(Rising Edge) and FED(Falling Edge) bits are set . This is enough to create an interrupt.
When the ECU is powered down and then the MCU receives a LIN wakeup request, the MCU can wake up thanks to the PMIC and LIN transceiver. But where I enable interrupts, I don't see RED and FED bits set, so the interrupt is not triggered. What could be the reason for this? In other words, Is there a possibility that RED and FED bits can be set by a wakeup request sent from the outside world without initializing LIN?
Show Less
Hi,
I want to send data from CANDUMP.log file to MCU. I am newly working on CAN receiver. Can anybody help me with the following things:
1. Do I have to use rxFIFO or rxbuffer to receive data continuously?
2. How do I assign rxbuffer and rxFIFO start address ?
3. How do I overwrite value in the memory when I receive continuous CAN messages?
I am using KIT_A2G_TC397_5V_TFT
I really appreciate it if you can share some CAN programming examples other than loopback mode example.
Thank you,
Show Less
Hello Team,
We are trying to configure ISR for PWM generation using ATOM for 3 channels. We are able to configure for one channel only and other two ATOM channels ISR is not working. Please let me know if you have any idea on the same.
configured ISR below for reference.
IFX_INTERRUPT(ATOM0Ch1_ISR, 0, ATOM0_CH1_PRIO)
{
}
Thank you
Show LessHi,
I am building app using tasking compiler, I am using #pragma pack(1) to avoid structure padding.
but I am facing this error ctc E209: #pragma pack: invalid number "(1)"
please let me know how to fix this or to suppress this error.
Thanks
g sai srinivas
Show Less
Hi This is Anand,
I am using IFX motor Development kit+ Drive Card
At Driver Card Part,
I have developed a sample code for GPIO toggling(Counter Machine is tri-core TC233LP)
I could able to flash the code by Bootstrap method(BAS) using Memtool.
But I am facing issue in debugging the code using Infineon DAP Miniwiggler V3.
These are the settings, that I have made at Driver card side,
Below is the Driver card Snapshot which I am using
1. Using external 5V0 DC supply to power ON(Below image, Option 3 is the Jumper/Fuse setting)-I could able to see Power up of board and able read 5V0 in multimeter on driver card i.e., X5 Terminal Block
2. Currently Fuse/Jumper is open at J2 and used Option 3 setting for J1 please comment on this FUSE/Jumper settings
3. After Launching Debug in Aurix IDE got the popup like this
Below is the connection setting in IDE,
4. Installed DAS server and Started the server
Getting No device(DAS JDS miniwiggler)
Below are the snapshot I am getting after starting the DAS Device scanner.
5.Getting Error Creating Session....
I am very new to this process and procedure.
Not able to sort-out ,
Expecting the support from community to help me out by providing the steps/procedure for debugging code in AURIX IDE using miniwiggler module.
(Also whether I need to install any supporting Drivers and software)
Tools that I have installed and using,
AURIX IDE,
Memtool and
DAS server
Thanks and Regards,
Ananda
Show Less
I have to synchronize three boards with a single master clock of 2 MHz. In addition, the three boards must work like this: two at 100kHz and one at 20 kHz.
How can I do this?
Thank you very much in advance.
Show Less