Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AURIX™ Forum Discussions

ramankant
AURIX™
I am testing Pflash read/write protection mechanism on Aurix TC3xx controller Evaluation board with with T32 debugger connected, I configured UCB_Pfla... Show More
yucheng
AURIX™
Hi infineon's friends: 请教个问题,TC387我们自己配置三相电流采样的时候, 发现V相(P33.7引脚)的采样结果一直比U/W 相的偏小, 查了下ADC的寄存器配置,没看出来三相有什么明显的差异。 希望能给予一些排查建议,谢谢!     Show More
yucheng
AURIX™
TC397 P33.14 这个脚我们用作GPIO,输出一个PWM信号给超声波雷达芯片, 当T14 (P33.14)这脚接到电平转换芯片时,会拉低VEVRSB这路供电。经过测量发现,T14 (P33.14)一接到电平转换芯片,VEVRSB这路电流会增加个60mA左右,导致外部35584 QST过流,V... Show More
Translation_Bot
AURIX™
About TLF35584 state machine Normal --> Sleep, tested and set WAK=0, ENA=0, SPI CMD (GoToSleep) failed to enter Sleep mode. Does MCU also need to be s... Show More
User20005
AURIX™
Hi,what is the reason interrupts are disabled in IfxQspi_SpiMaster_write() function? IfxCpu_disableInterrupts() is called at line 926 if DMA is used a... Show More
Galanoth
AURIX™
Hi, I am using SAK-TC367DP-64F300S AA in my project and supplying that MCU with TLF35584QVVS1 (5V variant). For the VDDP3 pins should I supply the pin... Show More
Dschunke
AURIX™
Hi guys, Has anybody here implemented Wake on CAN on Aurix TC399 (2nd gen triboard starter kit)? Could you please share any pointers for the same? Show More
sunji53
AURIX™

there is sentence "select ".[bd][sa][st]*" " in lsl file .  What's the meaning of [bd] [sa] and [st]?

P_xiaohui
AURIX™
  Hello everyone I have a question: _ COPY acts a PACKUP and is only evaluated if UCB Confirmation Code of_ ORIG is ERRORED or ERASED. W... Show More
Translation_Bot
AURIX™

How can I use AURIX to assist other SOCs to achieve functional safety design?

Forum Information

AURIX™

In this forum you can post your questions, comments and feedback about the 32-bit AURIX™ TriCore™ Microcontroller. The AURIX™ offers the highest scalability in performance, memory & peripherals across application. It is a safe and secure companion chip, meeting both the ISO functional safety standards and EVITA full security standards. Here you can also find the links to the latest board pages, SW and Tools GitHub, trainings, documents and FAQs