AURIX™ Forum Discussions
Hi team,
We are working with Aurix TC39x. We wanted to store 6byte value permanently in UCB_OTP. We have make it confirmed as we dont want to modify it further. We have read the OTP memory data which was stored earlier.
We are willing to from OTP region using Memtool. Can we have some guidelines to do so? As UCB
How can we read back the stored data in my project(ADS)? Any related examples, will help a lot.
Help is most appreciated.
Note: We are already having NDA with Infineon.
Regards,
Samad.
Show LessI downloaded the demo project "Application Kit TC397B" how can i build it in windows
i have already installed the bifaces
i met the following problems:
1 1_ToolEnv/0_Build/9_Make/0_Src/AppSw/i51/SubDirectory.mk:46: recipe for target '2_Out/i51_Keil/Keil_Files/0_Src/AppSw/i51/main.o' failed 命令语法不正确。
@mkdir -p $(@D)
Show LessDear members,
I am a beginner of MCU. I need to flash elf file into a TC39X chip, but I am using a MacBook with Apple M1 SOC. Do you have any advice for me to use tools like memtool so I can flash TC39X? Or I need to buy a windows laptop?
Thanks!
Show Less我尝试通过以下方式模拟触发相应Trap,但都没有成功,想请教一下,是什么原因。
1,触发:Class1 Tin2 - Memory Protection Read
模拟方式:(void) *(volatile uint32 *) (0x80008000);
没有发生trap。
Hi, when I used Lauterbach to debug TC397XP, I couldn't enter the main function after the code was burned. The phenomenon after burning the code is shown in the attachment. The power supply to the TC397XP is working fine. Also, ask if there were any other operations on the chip before using Lauterbach to burn the code for the first time.
Show Less
最近在使用TC234测试CAN模块,但是遇到了一个问题,当我使用CAN0模块的时候,节点0,1,2都可以正常收发数据,并且都能进入接收中断,但是当我将模块修改为CAN1模块使用CAN1模块的节点0,1,2的时候能将数据发出,查看NSR寄存器发现RXOK为1说明我接收到了数据,但是程序不会进入中断不知道是为什么,使用CAN0模块就可以进入中断,我只是修改了模块和引脚,对于输出中断线,CAN0范围是0~15,CAN1范围是0~7,我使用的接收中断是输出中断线3,一样不可以进入接收中断,只有CAN0模块可以进入中断,希望求助解决方法,学习学习,感谢
Show LessWhen using the KIT_MINIWIGGLER_3_USB burner on the TC397 board, there is a problem of not being able to connect.
It was discovered that as soon as the KIT_MINIWIGGLER_3_USB hardware is connected to the board, LED6 will stay bright when powered on (red, ESR0 pin is at a low level). As in the picture. Is there a problem with the burner? How can I fix it?.
log:
Message from component 'imtMemTool':
Can't connect to Target
Message from component 'controller0.core0.tc2coretargintf': Can't connect to target!
Message from component 'controller0.core0.tc2coretargintf': Can't connect target device via DAS!
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/TC397-%E5%85%AC%E6%9D%BF%E4%BD%BF%E7%94%A8KIT-MINIWIGGLER-3-USB-%E7%83%A7%E5%BD%95%E5%99%A8-%E5%87%BA%E7%8E%B0%E8%BF%9E%E6%8E%A5%E4%B8%8D%E4%B8%8A%E7%9A%84%E9%97%AE%E9%A2%98/td-p/641074
Show LessI'm Using TC364DP controller, I would like to know the State (Erased or Not) of the Particular PFlash Logical Sector .How can i get to know it is erased or not.
Is there any register for that ?
Hi,
Using the infineon-aurix_stm_interrupt_1_kit_tc397 routine added to the RTOS doesn't work, the interrupt cannot be triggered when the set time is reached, and there is no problem with the individual routine. What is the reason for this problem? Is it related to RTOS?
Thank you!
Show LessHello, Infineon Engineer
My question is mainly because he has used an STM32 MCU before, and he usually has a separate section in his data sheet explaining the conflict between pin multiplexes. For example, the three pins A, B, and C all have their own functions, but when A is configured with one of these functions, C cannot configure a certain function.
In the “Infineon-TC27xDC-Datasheet-v01_00-en” data sheet I have reviewed, I have not found a similar rule describing the location of pin multiplexing, as shown in the attachment. May I ask if the multiplexing pin function for each of the marked pins can be realized without any conflicts.
Other than that, I'd like to ask. Because this is my first time making a product. For the MCU, before soldering the finished board, I first solder a minimal system to solder the chip, write the program, then remove it and weld it to the finished board? Or do you write directly on the finished board?
Doublemint
2023.11.15
Show Less