Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

niko
Level 1
Level 1
First solution authored First reply posted First question asked

I am using the SPI bus of Aurix MCU TC397 to drive the audio decoding chip vs1053, and refer to the demo"SPI_ CPU_ 1_ KIT_ TC397_ TFT"。 This DEMO demonstrates how to use QSPI2 as the master and QSPI3 as the slave and send data from the master to the slave. These also works well in my project.
But how can I make the master read data from the slave? I tried to modify "g_Qspi.spiBuffers.spiSlaveTxBuffer" and "g_Qspi.spiBuffers.spiSlaveRxBuffer", but The correct data is still cannot be read from "g_Qspi.spiMasterTxBuffer" or "g_qspi.spiMasterRxBuffer" (I can only read 0x01 of the data sent before from the former, and 0x00 from the latter). And this phenomenon is different from what I observed on the oscilloscope.

0715c6a84011361fcbc46dfe01e654e.jpg


The blue line in the figure is MOSI, the green line is MISO, and the yellow line is CLK.
It can be seen that the data of MISO seems to be 0xff, which is not only has nothing to do with my settings in "g_Qspi.spiBuffers.spiSlaveTxBuffer". And also is irrelevant with The 0x00 read from "g_qspi.spiMasterRxBuffer" . This is what troubles me. It makes my master(TC397) unable to determine the status of the slave(vs1053).

0 Likes
1 Solution
niko
Level 1
Level 1
First solution authored First reply posted First question asked

yes, i generated my code based on the code above. However when i use the origin code, the master don't receive anything. So l write a function instead.like this:

/* This function starts the data transfer(1Byte) */
void SPI_transferByteData(uint8 *data)
{
while (IfxQspi_SpiSlave_getStatus(&g_qspi.spiSlave) == SpiIf_Status_busy ||
IfxQspi_SpiMaster_getStatus(&g_qspi.spiMasterChannel) == SpiIf_Status_busy)
{ /* Wait until the previous communication has finished, if any */
}
/* Send a data stream(Txbuffer) through the SPI Master and read slave into Rxbuffer*/
memcpy(&g_qspi.spiBuffers.spiMasterTxBuffer[0], data, SPI_BUFFER_SIZE);
IfxQspi_SpiMaster_exchange(&g_qspi.spiMasterChannel, &g_qspi.spiBuffers.spiMasterTxBuffer[0], &g_qspi.spiBuffers.spiMasterRxBuffer[0], SPI_BUFFER_SIZE);
memcpy(data, &g_qspi.spiBuffers.spiMasterRxBuffer[0], SPI_BUFFER_SIZE);
}

now it can send 1 byte while receive 1 byte .

View solution in original post

0 Likes
3 Replies
dw
Moderator
Moderator
Moderator
1000 replies posted 250 solutions authored 100 likes received
void transferData(void)
{
    while(IfxQspi_SpiSlave_getStatus(&g_qspi.spiSlave) == SpiIf_Status_busy ||
            IfxQspi_SpiMaster_getStatus(&g_qspi.spiMasterChannel) == SpiIf_Status_busy)
    {   /* Wait until the previous communication has finished, if any */
    }

    /* Instruct the SPI Slave to receive a data stream of defined length */
    IfxQspi_SpiSlave_exchange(&g_qspi.spiSlave, NULL_PTR, &g_qspi.spiBuffers.spiSlaveRxBuffer[0], SPI_BUFFER_SIZE);

    /* Send a data stream through the SPI Master */
    IfxQspi_SpiMaster_exchange(&g_qspi.spiMasterChannel, &g_qspi.spiBuffers.spiMasterTxBuffer[0], NULL_PTR, SPI_BUFFER_SIZE);

    verifyData();
}

Have you modified above code? pdf

0 Likes
niko
Level 1
Level 1
First solution authored First reply posted First question asked

yes, i generated my code based on the code above. However when i use the origin code, the master don't receive anything. So l write a function instead.like this:

/* This function starts the data transfer(1Byte) */
void SPI_transferByteData(uint8 *data)
{
while (IfxQspi_SpiSlave_getStatus(&g_qspi.spiSlave) == SpiIf_Status_busy ||
IfxQspi_SpiMaster_getStatus(&g_qspi.spiMasterChannel) == SpiIf_Status_busy)
{ /* Wait until the previous communication has finished, if any */
}
/* Send a data stream(Txbuffer) through the SPI Master and read slave into Rxbuffer*/
memcpy(&g_qspi.spiBuffers.spiMasterTxBuffer[0], data, SPI_BUFFER_SIZE);
IfxQspi_SpiMaster_exchange(&g_qspi.spiMasterChannel, &g_qspi.spiBuffers.spiMasterTxBuffer[0], &g_qspi.spiBuffers.spiMasterRxBuffer[0], SPI_BUFFER_SIZE);
memcpy(data, &g_qspi.spiBuffers.spiMasterRxBuffer[0], SPI_BUFFER_SIZE);
}

now it can send 1 byte while receive 1 byte .

0 Likes
dw
Moderator
Moderator
Moderator
1000 replies posted 250 solutions authored 100 likes received

Here list the original and modified for reference.

dw_0-1678071918778.png

 

0 Likes
This widget could not be displayed.