Why valid flag in GxRESDy of EVADC is not set?

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
chenpf321
Level 1
Level 1
5 replies posted 5 sign-ins First reply posted

Hi Support,

I'm using TC364 as uC, and I find that not all valid flag(VF) bits in register GxRESDy (x=0-11;y=0-15) of EVADC can be set 1 even if I can see the RESULT value updated as below. Is there any condition to set the valid flag? Thank you

 
 

chenpf321_3-1695029163165.png

 

chenpf321_0-1695029021801.png

 

0 Likes
1 Solution
Jeremy_Z
Moderator
Moderator
Moderator
1000 replies posted 250 sign-ins 100 likes received

Hi @chenpf321 
It seems a bit weird, and I was wondering if you could introduce the testing platform, such as board, demo code, debug tool, etc.
Further, whether you can replicate the phenomenon on these ADC demo codes.
BR,
Jeremy

View solution in original post

0 Likes
6 Replies
DownyK
Level 5
Level 5
100 replies posted 10 solutions authored 250 sign-ins

Hello @chenpf321 ,

Assuming normal conditions, the VF within the GxRESDy register will remain at 1 when no one approaches GxRESy with the new value updated in GxRESy.

If some code had read GxRESy, the corresponding VF would be changed to zero.

Did you happen to check if some code is not approaching GxRESy with a VF of 0?

thank you.

0 Likes

Hi DownyK,

The codes only read the VF of GxRESy, not the RESULT of GxRESy. So VF should not be cleared.

Using debugger can only see GxRESDy value, in the picture above, VF is also not set.

0 Likes
Jeremy_Z
Moderator
Moderator
Moderator
1000 replies posted 250 sign-ins 100 likes received

Hi @chenpf321 
Whether you mean the VF bit of the corresponding GxRESDy will be cleared after the code reads the VF of GxRESy, is it right?
If yes, can you share the related codes?
BR,
Jeremy

0 Likes
Jeremy_Z
Moderator
Moderator
Moderator
1000 replies posted 250 sign-ins 100 likes received

Hi @chenpf321 
It seems a bit weird, and I was wondering if you could introduce the testing platform, such as board, demo code, debug tool, etc.
Further, whether you can replicate the phenomenon on these ADC demo codes.
BR,
Jeremy

0 Likes
chenpf321
Level 1
Level 1
5 replies posted 5 sign-ins First reply posted

Hi Jeremy,

Sorry that I don't have the testing board right now

0 Likes
Jeremy_Z
Moderator
Moderator
Moderator
1000 replies posted 250 sign-ins 100 likes received

Hi @chenpf321 ,

How're things going?

BR,

Jeremy

0 Likes