Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User18151
Level 3
Level 3
First like received First solution authored
Hi all,

Which operating systems are supported by MemTool?

Kind regards,
Christine

#8042000 21013
0 Likes
2 Replies
User13836
Level 6
Level 6
50 likes received 50 solutions authored 100 sign-ins
Hi Christine,

tjhe Infineon Memtool 4 (v4.7) Overview page which is included in the memtool documentation (file IMTMemtool.chm included in the help sub folder of the memtool installation folder) reveals the following information:

Infineon Memtool 4 can be used on PC's running Microsoft Windows2000, WindowsXP Pro, Windows Vista or Windows 7. The target is connected to the host PC using DAS Wigler or a standard RS232 port.

I'm using this memtool version successfully on a Win 10 64 bit PC. So Win 10 is also working, although not included in the online help section.

Best regards,
Ulrich Kloidt

TASKING tools support
0 Likes
User18237
Level 5
Level 5
First solution authored First like received
Hi Christine,

Supported operating systems are shown in the release notes of the MemTool.
e.g.
In the MemTool version: 4.8.1 (11.10.2019), the following operating systems are supported.
Microsoft Windows™ Vista
Microsoft Windows™ 7 ( 32-bit (x86) or 64-bit (x64) versions )
Microsoft Windows™ 8.1 ( 32-bit (x86) or 64-bit (x64) versions )
Microsoft Windows™ 10 ( 32-bit (x86) or 64-bit (x64) versions )
Note: You need administrator permissions to install the program.

Kind regards,
Mr. AURIX™
0 Likes