Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

User17740
Level 3
Level 3
First like received
Hi all,

Which datasheet parameters are related to the specific pins/balls?

Kind regards,
Bernie

#8042000 12885
0 Likes
1 Reply
User18237
Level 5
Level 5
First solution authored First like received
Hi Bernie,

Pinning information is shown in chapter “Package and Pinning Definitions” in the datasheet.
There are tables for each ports functions (e.g. Port 00 Functions) for each packages (e.g. BGA516).
In the table, the buffer type for each pins/balls are shown in column “Type” by abbreviations which are defined in Legend located at the end of the tables.
The datasheet parameters related to the types are shown in chapter “Electrical Specification”.
Example: TC299x BGA516 Package, ball “M6”
Based on the table, type is MP/PU1/VEXT.
Based on the legend,
MP = Pad class MP (5V/3.3V)
PU1 = with pull-up device connected during reset (PORST = 0) with footnotes 1) 2) 3)
Vx = Supply
The parameters related to the pad class ”MP” and supply “VEXT” are shown in chapter “Electrical Specification”.

Kind regards,
Mr. AURIX™
0 Likes