What is the state of Port Pins during and after /PORST activation in AURIX™ ?

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User17612
Level 4
Level 4
First like received
Hi,

What is the state of Port Pins during and after /PORST activation in AURIX™?

Kind regards,
Lucas

#8042000 13144
0 Likes
1 Reply
User18237
Level 5
Level 5
First solution authored First like received
Hi Lucas,

For TC26x, TC27x and TC29x, there are two options (Pull up or Tristate) available, depending on the selection of HWCFG6 pin (P14.4).
With HWCFG6 = 1, all port pins except P33.8 and P40.x are set to pull-up mode.
With HWCFG6 = 0, all port pins except P33.8 and P40.x are set to tristate mode.
Port pins P33.8 and P40.x are in tristate mode during and after /PORST activation.
For TC21x, TC22x and TC23x, all port pins are in Tristate mode during and after /PORST activation. No HWCFG6 selection available.
For details on certain dedicated pins reset behavior (ie, /TESTMODE, /ESRx), please refer to device datasheets chapter -> Pull-Up/Pull-Down Reset Behavior of the Pins.

Best regards,
Mr. AURIX™
0 Likes