What is the CC or SR in column “Symbol” in electrical specification parameters in the

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User17740
Level 4
Level 4
First solution authored First like received
Hi,

What is the CC or SR in column “Symbol” in electrical specification parameters in the datasheet?

Kind regards,
Bernie

#8042000 12876
0 Likes
1 Reply
User18237
Level 5
Level 5
First solution authored First like received
Hi Bernie,

The parameters listed in Electrical Specification partly represent the characteristics of the microcontroller and partly its requirements on the system. To aid interpreting the parameters easily when evaluating them for a design, they are marked with an two-letter abbreviation in column “Symbol”:
• CC
Such parameters indicate Controller Characteristics which are a distinctive feature of the microcontroller and must be regarded for a system design.
• SR
Such parameters indicate System Requirements which must be provided by the microcontroller system in which the microcontroller designed in.

Kind regards,
Mr. AURIX™
0 Likes