Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

User18303
Level 2
Level 2
Hi all,

could you please tell me what is Memtool?

Thanks!
Lina


#8042000 13343
0 Likes
1 Reply
User18237
Level 5
Level 5
First solution authored First like received
Hi Lina,


The Infineon MemTool is a free-of-charge PC/Windows based software for on-chip flash programming. The software supports all Infineon Microcontroller devices
According to the capabilities of the on-chip flash device, MemTool can be used to erase, program, verify, and protect selectable flash sections or perform these functions on the complete program and data flash areas.
MemTool provide ready-to-use configuration files for the complete range of Infineon Microcontroller evaluation boards and application kits and allows PC/Windows USB-to-target connections via DAS and UART. DAP and JTAG connections to the target system can be performed together with the Infineon miniWiggler.

Please try to download and install the latest version of Memtool to ensure the support of new Infineon microcontroller derivatives.


Best regards
Mr. AURIX™
0 Likes