Announcements

Equip yourself to optimize AURIX™ MCUs for Evs at the EV Webinar. Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

pistons7
Level 3
Level 3
5 likes given First solution authored 10 replies posted

I use the below sample program.

https://community.infineon.com/t5/Code-Examples/Sample-code-using-ADS-for-the-TC334-to-enter-Standby...

I do not use LED program , instead, the CAN communication function is used so that the status can be confirmed by transmitting CAN when in the NORMAL state.

Also, to use SCR as a wakeup trigger, I made the following modifications.

standbyConfig.enableScr = TRUE;

standbyConfig.enableWakeupOnScr = TRUE;

 

SCR is the following program.

void main(void)
{

SCR_SCU_PAGE = 1; //Switch to page 1
SCR_PMCON1 =0x3B; //OCDS, T2CCU and SSC enabled

SCR_SCU_PAGE = 0; //Switch to page 0
SCR_IRCON0 = 0x0; //Reset interrupts

SCR_IEN0 = 0x80; //Enable global interrupts
SCR_IEN1 = 0x80; //XINTR13 is enabled

SCR_SCU_PAGE = 1;
SCR_RTC_CNT3 = 0;
SCR_RTC_CNT2 = 0;
SCR_RTC_CNT1 = 0;
SCR_RTC_CNT0 = 0;

SCR_RTC_RTCCR3 = 0x00;
SCR_RTC_RTCCR2 = 0x00;
SCR_RTC_RTCCR1 = 0xFF;
SCR_RTC_RTCCR0 = 0x40;
SCR_RTC_RTCON = 0x15;

while(1)
{
}
}

void __interrupt(0x6B) rtc_interrupt(void)
{

SCR_SCU_PAGE = 1;
SCR_SCU_STDBYWKP = 0x2;

}

I confirmed that it will be in Standby mode. But I can't wake up from SCR.
Where am I going wrong?

 

 

0 Likes
2 Replies
Prudhvi
Moderator
Moderator
Moderator
50 solutions authored 250 sign-ins 10 likes given

Hello,

Could you please clarify how you're trying to perform a wakeup? The TC3xx_UM_Part_1 section "11.2.3.4 Standby Mode" mentioned about different ways to wake up from Standby mode under different configurations of VEXT and VEVRSB.

Regards,

Prudhvi.

Hello.

[premise] Standby Mode with both VEXT and VEVRSB supplied via common supply rail(PMIC)

 

I want to wake-up via "Wake-up is triggered by Standby ControlleR if configured via PMSWCR0.SCRWKEN enable bit."

And in SCR, I want to use RTC to generate an interrupt and wake up after a certain period of time.

 

Regards,

Pistons7

 

 

 

0 Likes