Voltage range of VDDPD in TC365DP

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Hyma_Varghese
Level 1
Level 1
First question asked Welcome!

Hi,
In Infineon-AURIX_TC3xx_Part1-UserManual-v02_00-EN.pdf, the VDDPD voltage range provided in table 290 is conflicting with the voltage range provided in Figure 113, Table 284 and Table 285. Please confirm the correct voltage range of supply voltage VDDPD.
Table 290: 1.125V -1.375V
Table 284: 1.15V - 1.43V
Table 285: 1.15V - 1.43V
Figure 113: 1.15V - 1.43V, PREOVVAL range: 1.43V – 1.48V, PREUVVAL range: 1.1V – 1.15V

Best Regards,
Hyma Varghese

0 Likes
1 Reply
Aiswarya_A
Moderator
Moderator
Moderator
25 likes received 250 sign-ins 50 solutions authored

Hello,

Could you please check "4.76 [PMS_TC.H003] VDDPD voltage monitoring limits" in the TC36x_AA_Errata_Sheet_v2_0 ?
You could also check this thread

Kind Regards,
Aiswarya.

0 Likes