Using DAS/Memtool with Lauterbach emulator

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Fabien
Level 1
Level 1
First solution authored First reply posted First like given

Hello,

 

I am using a TC222 evalboard with a LA-2707 Tricore Automotive PRO dongle plugged on DAP used for debugging. Debug is working by using Trace 32 tool.

 

To be able to change the UCBs, i need to connect to the evalboard by using MemTool and DAS. But, as you can see in the screenshot below, Lauterbach connector is connected to the PC, but DAS does not see it.

Fabien_0-1663313485127.png

 

Is DAS compatible with Lauterbach probe, or only with miniwriggler? If it is compatible, how to setup DAS?

 

Thank you.

 

Best regards.

0 Likes
1 Solution
µC_Wrangler
Employee
Employee
50 solutions authored 100 sign-ins 25 likes received

Hi @Fabien .  DAS only works with a USB connection through the FTDI chip on the TriBoard, or with a miniWiggler.  The Lauterbach USB device is not supported by DAS.

You can also change UCBs via scripts in Trace32.

View solution in original post

2 Replies
µC_Wrangler
Employee
Employee
50 solutions authored 100 sign-ins 25 likes received

Hi @Fabien .  DAS only works with a USB connection through the FTDI chip on the TriBoard, or with a miniWiggler.  The Lauterbach USB device is not supported by DAS.

You can also change UCBs via scripts in Trace32.

Fabien
Level 1
Level 1
First solution authored First reply posted First like given

OK, thank you.

0 Likes