Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
BluewindAZ
Level 1
Level 1
5 sign-ins First question asked Welcome!
With particular reference to AURIX 2G TC3xx (but also applies to AURIX 1G),
all PSPR and DSPR segments of all cores are accessible from all cores, directly or via cross-bar.
The difference is in terms of performance.
In general, the recommendation is to store the code executed by CORE 0 in PFLASH 0, the code executed by CORE 1 in PFLASH 1, etc ...; with this recommendation you can run your code faster.
It's also recommended to use PSPR for the code and DSPR for the data, for example executing code from DSPR is possible but will result in additional wait states.
If I want to use a PSPR for data, for example PSPR 2 to place a stack used by CORE 0,
is it correct to say that "as long as you accept a performance degradation, PSPRx can also be used for data"?
0 Likes
1 Solution
MoD
Employee
Employee
10 likes given 50 likes received 500 replies posted
Yes, it is correct to say that "as long as you accept a performance degradation, PSPRx can also be used for data"

View solution in original post

0 Likes
1 Reply
MoD
Employee
Employee
10 likes given 50 likes received 500 replies posted
Yes, it is correct to say that "as long as you accept a performance degradation, PSPRx can also be used for data"
0 Likes