Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

Not applicable
Hello,
I want to interface two sensor on one bus line by SPC protocol, So i will use single pin as input and output. So how should be the declaration of pin as input or output (in manual it is written as quasi bidirection )
And how should i generate the trigger pulse for selection of one sensor according to address.

Can any one please help in this regards
Thanks
0 Likes
1 Reply
MoD
Employee
Employee
250 sign-ins 25 likes received 50 solutions authored
Hello,
the pin must be set to corresponding alternate output (SPC) with open drain. External pull up is needed. Trigger pulses can be generated by write to SENT_SCRx register. See chapter SPC Operation for more Information in the device user manual.
0 Likes