Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

User15824
Level 1
Level 1
Hi,

I have tried to test the bus-off status (CAN_H shortened to CAN_L)

In my case the registry ECNT.LEC is taking the value 101 (bit0 error) and the CB.INIT is 1 (deactivate state), both registers TEC and REC remains 0. The BOFF bit remains inactive.

To recover the bus, when the error condition disappear, is needed to activate the node with CB.INIT is 0...

The question here is:

In the above description, why the CAN bus does not fall in bus-off?

Thanks...
Adel
0 Likes
1 Reply
ugo_8a
Employee
Employee
10 solutions authored 25 sign-ins 25 replies posted
You need to transmit periodically a message from the uC, if you have a CAN monitor tool is recommended to used as listener only so when you apply the short
the monitor tool does not go to BusOff as well
0 Likes
This widget could not be displayed.