- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Cannot figure out, why is my file (containing only DataFlash0 byte defines) linked into the output hex twice. I am compiling for Infineon TC1797 with Tasking VX compiler.
Besides the program, I have a file named data_flash_bank_0.asm, which only includes predefined data bytes.
Compiler properly places it at the expected address of 0x8FE00000, which is the data flash 0 in hardware.
What is wrong is that the same code appears within the program as a second copy, wasting space and not wanted.
All the setting in the project properties seems fine, 'delete duplicate' enabled.
To illustrate the problem, I made one VERY SMALL project, where there are only 3 files: test.c function with main(), short assembly function reading the data flash, and the data flash predefines.
test.c:
#include <stdio.h>
extern void * loop_36(void); // call the main assembly function
int main(void)
{
loop_36();
}
assembly function jozo.asm:
.sdecl "PFLASH", CODE
.sect "PFLASH"
.global loop_36
loop_36:
movh.a a4, #0x8FE0
mov16 d2, #0 ; Move
lea a2, 0x3F ; Load Effective Address
loop:
ld16.w d15, [a4+]4 ; Load Word
or.ne d2, d15, #0 ; Not Equal Accumulating
loop16 a2, loop ; Loop
ret16 ; Return from Call
.end
and the actual predefined bytes area giving me the problem, file data_flash_bank_0.asm:
.sdecl ".data.dflash0", DATA AT 0x8FE00000
.sect ".data.dflash0" ; new edit: trying .rodata instead of .data
.byte 0xF2, 0x45, .... 32k more bytes
.end
Map file: (the last line is what I expect, but the 2 lines above it, also length 0x8000, I do not want)
+------------------------------------------------------------------------------------------------------------------------+
| Chip | Group | Section | Size (MAU) | Space addr | Chip addr | Alignment |
| ========================================================================================================================|
| spe:pflash0 | | .text._Exit.libc (191) | 0x00000004 | 0x80000008 | 0x00000008 | 0x00000008 |
| spe:pflash0 | | .text._c_init.libcs_fpu (98) | 0x0000000c | 0x8000000c | 0x0000000c | 0x00000002 |
| spe:pflash0 | | .text._c_init_entry.libcs_fpu (97) | 0x00000132 | 0x80000020 | 0x00000020 | 0x00000020 |
| spe:pflash0 | | table (202) | 0x00000030 | 0x80000154 | 0x00000154 | 0x00000004 |
| spe:pflash0 | | .text._ldmst_clear_byte.libcs_fpu (95) | 0x0000002e | 0x80000184 | 0x00000184 | 0x00000002 |
| spe:pflash0 | | .text._ldmst_copy_byte.libcs_fpu (96) | 0x00000044 | 0x800001b2 | 0x000001b2 | 0x00000002 |
| spe:pflash0 | | .text.cstart..cocofun_1 (14) | 0x0000001a | 0x800001f6 | 0x000001f6 | 0x00000002 |
| spe:pflash0 | | .text.cstart.__init_sp (12) | 0x0000001c | 0x80000210 | 0x00000210 | 0x00000002 |
| spe:pflash0 | | .text.cstart._start (13) | 0x000001c2 | 0x8000022c | 0x0000022c | 0x00000002 |
| spe:pflash0 | | .text.sync_on_halt._sync_on_halt (61) | 0x0000008e | 0x800003ee | 0x000003ee | 0x00000002 |
| spe:pflash0 | | .text.sync_on_halt._sync_on_halt_end (60) | 0x0000000c | 0x8000047c | 0x0000047c | 0x00000002 |
| spe:pflash0 | | .text.test.main (84) | 0x0000000c | 0x80000488 | 0x00000488 | 0x00000002 |
| spe:pflash0 | | [.data.dflash0] (203) | 0x00008000 | 0x80000494 | 0x00000494 | 0x00000001 |
| spe:pflash0 | | PFLASH (5) | 0x00000014 | 0x80008494 | 0x00008494 | 0x00000001 |
| spe:dflash0 | | .data.dflash0 (1) | 0x00008000 | 0x8fe00000 | 0x0 | 0x00000001 |
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Walt,
please add the rom keyword to the data definition. I suggest to follow the Infineon EABI spec which requires to use the section name prefix .rodata for constant, far accessed data:
.sdecl ".rodata.dflash0", DATA, ROM AT 0x8FE00000
.sect ".rodata.dflash0" ;
If ROM is omitted, the linker will treat the data as initialized data and create a ROM copy for the initialization when the linker generated copy table is processed during the C startup code execution.
Best regards,
Ulrich Kloidt
TASKING Tools support
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi walt,
I have used Bifaces and Tasking to add your asm code into Dflash0, and below is a 2 byte example.
dw
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Walt,
please add the rom keyword to the data definition. I suggest to follow the Infineon EABI spec which requires to use the section name prefix .rodata for constant, far accessed data:
.sdecl ".rodata.dflash0", DATA, ROM AT 0x8FE00000
.sect ".rodata.dflash0" ;
If ROM is omitted, the linker will treat the data as initialized data and create a ROM copy for the initialization when the linker generated copy table is processed during the C startup code execution.
Best regards,
Ulrich Kloidt
TASKING Tools support