- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The LED0 don not light and i use the device can not receive the message.
//////////////////////////////////////////////////////////
#include "Ifx_Types.h"
#include "IfxCpu.h"
#include "IfxScuWdt.h"
IFX_ALIGN(4) IfxCpu_syncEvent g_cpuSyncEvent = 0;
#include "Ifx_Types.h"
#include "IfxCan_Can.h"
#include "IfxCan.h"
#include "IfxCpu_Irq.h"
#include "IfxPort.h"
#include "Bsp.h"
#define LED0 &MODULE_P13,0
#define LED1 &MODULE_P13,1
#define LED2 &MODULE_P13,2
#define LED3 &MODULE_P13,3
#define MODULE_CAN0_RAM 0xF0200000
#define NODE0_RAM_OFFSET 0x0
//#define NODE1_RAM_OFFSET 0x1000
#define CAN_MESSAGE_TX_ID0 (uint32)0x1234567
#define CAN_MESSAGE_RX_ID1 (uint32)0x1234561
#define CAN_MESSAGE_RX_ID2 (uint32)0x1234562
#define CAN_MESSAGE_RX_ID3 (uint32)0x1234563
#define ISR_PRIORITY_CAN_TX 2 /* Define the CAN TX interrupt priority */
#define ISR_PRIORITY_CAN_RX 1 /* Define the CAN RX interrupt priority */
#define MAXIMUM_CAN_DATA_PAYLOAD 2 /* Define maximum classical CAN payload in 4-byte words */
IFX_CONST IfxCan_Can_Pins Can00_pins = {
&IfxCan_TXD00_P20_8_OUT, IfxPort_OutputMode_pushPull, // CAN00_TX
&IfxCan_RXD00B_P20_7_IN, IfxPort_InputMode_pullUp, // CAN00_RX
IfxPort_PadDriver_cmosAutomotiveSpeed4
};
typedef struct
{
IfxCan_Can_Config canConfig; /* CAN module configuration structure */
IfxCan_Can canModule; /* CAN module handle */
IfxCan_Can_Node can00Node; /* CAN source node handle data structure */
IfxCan_Can_NodeConfig canNodeConfig; /* CAN node configuration structure */
IfxCan_Filter canFilter; /* CAN filter configuration structure */
IfxCan_Message txMsg; /* Transmitted CAN message structure */
IfxCan_Message rxMsg; /* Received CAN message structure */
uint32 txData[MAXIMUM_CAN_DATA_PAYLOAD]; /* Transmitted CAN data array */
uint32 rxData[MAXIMUM_CAN_DATA_PAYLOAD]; /* Received CAN data array */
} McmcanType;
McmcanType g_mcmcan;
IFX_INTERRUPT(canIsrTxHandler, 0, ISR_PRIORITY_CAN_TX);
void canIsrTxHandler(void)
{
/* Clear the "Transmission Completed" interrupt flag */
IfxCan_Node_clearInterruptFlag(g_mcmcan.can00Node.node, IfxCan_Interrupt_transmissionCompleted);
IfxPort_togglePin(LED0); //transmit indicator
}
IFX_INTERRUPT(canIsrRxHandler, 0, ISR_PRIORITY_CAN_RX);
void canIsrRxHandler(void)
{
/* Clear the "Message stored to Dedicated RX Buffer" interrupt flag */
IfxCan_Node_clearInterruptFlag(g_mcmcan.can00Node.node, IfxCan_Interrupt_messageStoredToDedicatedRxBuffer);
/* Clear the "New Data" flag; as long as the "New Data" flag is set, the respective Rx buffer is
* locked against updates from received matching frames.
*/
IfxCan_Node_clearRxBufferNewDataFlag(g_mcmcan.can00Node.node, g_mcmcan.canFilter.rxBufferOffset);
/* Read the received CAN message */
IfxCan_Can_readMessage(&g_mcmcan.can00Node, &g_mcmcan.rxMsg, g_mcmcan.rxData);
/* Check if the received data matches with the transmitted one */
if((g_mcmcan.rxMsg.messageId == CAN_MESSAGE_RX_ID1)
&& (g_mcmcan.rxData[1] == 0xEFCDAB89))
{
if(g_mcmcan.rxData[0] == 0x67452301) { //send 0x
IfxPort_setPinState(LED1, IfxPort_State_low); //LED ON
} else {
IfxPort_setPinState(LED1, IfxPort_State_high); //LED OFF
}
}
if((g_mcmcan.rxMsg.messageId == CAN_MESSAGE_RX_ID2)
&& (g_mcmcan.rxData[1] == 0xEFCDAB89))
{
if(g_mcmcan.rxData[0] == 0x67452302) {
IfxPort_setPinState(LED2, IfxPort_State_low);
} else {
IfxPort_setPinState(LED2, IfxPort_State_high);
}
}
if((g_mcmcan.rxMsg.messageId == CAN_MESSAGE_RX_ID3)
&& (g_mcmcan.rxData[1] == 0xEFCDAB89))
{
if(g_mcmcan.rxData[0] == 0x67452303) {
IfxPort_setPinState(LED3, IfxPort_State_low);
} else {
IfxPort_setPinState(LED3, IfxPort_State_high);
}
}
}
void initCAN0(void)
{
/*******CAN module configuration and initialization*******/
IfxCan_Can_initModuleConfig(&g_mcmcan.canConfig, &MODULE_CAN0);
IfxCan_Can_initModule(&g_mcmcan.canModule, &g_mcmcan.canConfig);
/*******CAN00 node configuration and initialization*******/
IfxCan_Can_initNodeConfig(&g_mcmcan.canNodeConfig, &g_mcmcan.canModule);
g_mcmcan.canNodeConfig.nodeId = IfxCan_NodeId_0;
g_mcmcan.canNodeConfig.clockSource = IfxCan_ClockSource_both;
g_mcmcan.canNodeConfig.frame.type = IfxCan_FrameType_transmitAndReceive;
g_mcmcan.canNodeConfig.frame.mode = IfxCan_FrameMode_standard; //Classic CAN
g_mcmcan.canNodeConfig.txConfig.txMode = IfxCan_TxMode_dedicatedBuffers;
g_mcmcan.canNodeConfig.txConfig.dedicatedTxBuffersNumber = 255;
g_mcmcan.canNodeConfig.txConfig.txBufferDataFieldSize = IfxCan_DataFieldSize_8;
g_mcmcan.canNodeConfig.rxConfig.rxMode = IfxCan_RxMode_dedicatedBuffers;
g_mcmcan.canNodeConfig.rxConfig.rxBufferDataFieldSize = IfxCan_DataFieldSize_8;
g_mcmcan.canNodeConfig.filterConfig.extendedListSize = 255; //Extended Frame
g_mcmcan.canNodeConfig.filterConfig.messageIdLength = IfxCan_MessageIdLength_extended;
g_mcmcan.canNodeConfig.messageRAM.extendedFilterListStartAddress = 0x100; //Extended Frame
g_mcmcan.canNodeConfig.messageRAM.rxBuffersStartAddress = 0x200;
g_mcmcan.canNodeConfig.messageRAM.txBuffersStartAddress = 0x400;
g_mcmcan.canNodeConfig.messageRAM.baseAddress = MODULE_CAN0_RAM + NODE0_RAM_OFFSET;
g_mcmcan.canNodeConfig.baudRate.baudrate = 500000; //500KBaud
//transmit interrupt
g_mcmcan.canNodeConfig.interruptConfig.transmissionCompletedEnabled = TRUE;
g_mcmcan.canNodeConfig.interruptConfig.traco.priority = ISR_PRIORITY_CAN_TX;
g_mcmcan.canNodeConfig.interruptConfig.traco.interruptLine = IfxCan_InterruptLine_0;
g_mcmcan.canNodeConfig.interruptConfig.traco.typeOfService = IfxSrc_Tos_cpu0;
//receive interrupt
g_mcmcan.canNodeConfig.interruptConfig.messageStoredToDedicatedRxBufferEnabled = TRUE;
g_mcmcan.canNodeConfig.interruptConfig.reint.priority = ISR_PRIORITY_CAN_RX;
g_mcmcan.canNodeConfig.interruptConfig.reint.interruptLine = IfxCan_InterruptLine_1;
g_mcmcan.canNodeConfig.interruptConfig.reint.typeOfService = IfxSrc_Tos_cpu0;
//binding pin
g_mcmcan.canNodeConfig.pins = &Can00_pins;
IfxCan_Can_initNode(&g_mcmcan.can00Node, &g_mcmcan.canNodeConfig);
/*******CAN filter configuration and initialization*******/
g_mcmcan.canFilter.number = 0;
g_mcmcan.canFilter.elementConfiguration = IfxCan_FilterElementConfiguration_storeInRxBuffer;
g_mcmcan.canFilter.id1 = CAN_MESSAGE_RX_ID1;
g_mcmcan.canFilter.rxBufferOffset = IfxCan_RxBufferId_0;
//IfxCan_Can_setStandardFilter(&g_mcmcan.can00Node, &g_mcmcan.canFilter);
IfxCan_Can_setExtendedFilter(&g_mcmcan.can00Node, &g_mcmcan.canFilter);
g_mcmcan.canFilter.number = 1;
g_mcmcan.canFilter.elementConfiguration = IfxCan_FilterElementConfiguration_storeInRxBuffer;
g_mcmcan.canFilter.id1 = CAN_MESSAGE_RX_ID2;
//g_mcmcan.canFilter.id2 = CAN_MESSAGE_RX_ID2;
g_mcmcan.canFilter.rxBufferOffset = IfxCan_RxBufferId_0;
//IfxCan_Can_setStandardFilter(&g_mcmcan.can00Node, &g_mcmcan.canFilter);
IfxCan_Can_setExtendedFilter(&g_mcmcan.can00Node, &g_mcmcan.canFilter);
g_mcmcan.canFilter.number = 2;
g_mcmcan.canFilter.elementConfiguration = IfxCan_FilterElementConfiguration_storeInRxBuffer;
g_mcmcan.canFilter.id1 = CAN_MESSAGE_RX_ID3;
//g_mcmcan.canFilter.id2 = CAN_MESSAGE_RX_ID3;
g_mcmcan.canFilter.rxBufferOffset = IfxCan_RxBufferId_0;
//IfxCan_Can_setStandardFilter(&g_mcmcan.can00Node, &g_mcmcan.canFilter);
IfxCan_Can_setExtendedFilter(&g_mcmcan.can00Node, &g_mcmcan.canFilter);
}
void initLED(void)
{
IfxPort_setPinMode(LED0, IfxPort_Mode_outputPushPullGeneral); /* Initialize LED port pin */
IfxPort_setPinMode(LED1, IfxPort_Mode_outputPushPullGeneral);
IfxPort_setPinMode(LED2, IfxPort_Mode_outputPushPullGeneral);
IfxPort_setPinMode(LED3, IfxPort_Mode_outputPushPullGeneral);
IfxPort_setPinState(LED0, IfxPort_State_high); /* Turn off LED (LED is low-level active) */
IfxPort_setPinState(LED1, IfxPort_State_high);
IfxPort_setPinState(LED2, IfxPort_State_high);
IfxPort_setPinState(LED3, IfxPort_State_high);
}
void core0_main(void)
{
IfxCpu_enableInterrupts();
/* !!WATCHDOG0 AND SAFETY WATCHDOG ARE DISABLED HERE!!
* Enable the watchdogs and service them periodically if it is required
*/
IfxScuWdt_disableCpuWatchdog(IfxScuWdt_getCpuWatchdogPassword());
IfxScuWdt_disableSafetyWatchdog(IfxScuWdt_getSafetyWatchdogPassword());
/* Wait for CPU sync event */
IfxCpu_emitEvent(&g_cpuSyncEvent);
IfxCpu_waitEvent(&g_cpuSyncEvent, 1);
initLED();
initTime();
initCAN0();
IfxCan_Can_initMessage(&g_mcmcan.txMsg);
g_mcmcan.txMsg.messageId = CAN_MESSAGE_TX_ID0;
g_mcmcan.txMsg.bufferNumber = 0;
g_mcmcan.txMsg.dataLengthCode = IfxCan_DataLengthCode_8;//8 bytes
g_mcmcan.txMsg.frameMode = IfxCan_FrameMode_standard; //Classic CAN
g_mcmcan.txMsg.messageIdLength=IfxCan_MessageIdLength_extended; //Extended Frame
g_mcmcan.txData[0] = 0x98BADCFE;
g_mcmcan.txData[1] = 0x10325476;
//you will receive: FE DC BA 98 76 54 32 10
while(1)
{
while(IfxCan_Status_notSentBusy ==
IfxCan_Can_sendMessage(&g_mcmcan.can00Node, &g_mcmcan.txMsg, &g_mcmcan.txData[0]) );
waitTime(TimeConst_1s);
}
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Please refer to this example code, and a separated slide send to your email.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
//There are two nodes used, one is for transamiting, the other is for receiving.
void initMcmcan(void)
{
/* ==========================================================================================
* CAN module configuration and initialization:
* ==========================================================================================
* - load default CAN module configuration into configuration structure
* - initialize CAN module with the default configuration
* ==========================================================================================
*/
IfxCan_Can_initModuleConfig(&g_mcmcan.canConfig, &MODULE_CAN0);
IfxCan_Can_initModule(&g_mcmcan.canModule, &g_mcmcan.canConfig);
/* ==========================================================================================
* Source CAN node configuration and initialization:
* ==========================================================================================
* - load default CAN node configuration into configuration structure
*
* - set source CAN node in the "Loop-Back" mode (no external pins are used)
* - assign source CAN node to CAN node 0
*
* - define the frame to be the transmitting one
*
* - once the transmission is completed, raise the interrupt
* - define the transmission complete interrupt priority
* - assign the interrupt line 0 to the transmission complete interrupt
* - transmission complete interrupt service routine should be serviced by the CPU0
*
* - initialize the source CAN node with the modified configuration
* ==========================================================================================
*/
IfxCan_Can_initNodeConfig(&g_mcmcan.canNodeConfig, &g_mcmcan.canModule);
g_mcmcan.canNodeConfig.busLoopbackEnabled = TRUE;
g_mcmcan.canNodeConfig.nodeId = IfxCan_NodeId_0;
g_mcmcan.canNodeConfig.frame.type = IfxCan_FrameType_transmit;
g_mcmcan.canNodeConfig.interruptConfig.transmissionCompletedEnabled = TRUE;
g_mcmcan.canNodeConfig.interruptConfig.traco.priority = ISR_PRIORITY_CAN_TX;
g_mcmcan.canNodeConfig.interruptConfig.traco.interruptLine = IfxCan_InterruptLine_0;
g_mcmcan.canNodeConfig.interruptConfig.traco.typeOfService = IfxSrc_Tos_cpu0;
IfxCan_Can_initNode(&g_mcmcan.canSrcNode, &g_mcmcan.canNodeConfig);
/* ==========================================================================================
* Destination CAN node configuration and initialization:
* ==========================================================================================
* - load default CAN node configuration into configuration structure
*
* - set destination CAN node in the "Loop-Back" mode (no external pins are used)
* - assign destination CAN node to CAN node 1
*
* - define the frame to be the receiving one
*
* - once the message is stored in the dedicated RX buffer, raise the interrupt
* - define the receive interrupt priority
* - assign the interrupt line 1 to the receive interrupt
* - receive interrupt service routine should be serviced by the CPU0
*
* - initialize the destination CAN node with the modified configuration
* ==========================================================================================
*/
IfxCan_Can_initNodeConfig(&g_mcmcan.canNodeConfig, &g_mcmcan.canModule);
g_mcmcan.canNodeConfig.busLoopbackEnabled = TRUE;
g_mcmcan.canNodeConfig.nodeId = IfxCan_NodeId_1;
g_mcmcan.canNodeConfig.frame.type = IfxCan_FrameType_receive;
g_mcmcan.canNodeConfig.interruptConfig.messageStoredToDedicatedRxBufferEnabled = TRUE;
g_mcmcan.canNodeConfig.interruptConfig.reint.priority = ISR_PRIORITY_CAN_RX;
g_mcmcan.canNodeConfig.interruptConfig.reint.interruptLine = IfxCan_InterruptLine_1;
g_mcmcan.canNodeConfig.interruptConfig.reint.typeOfService = IfxSrc_Tos_cpu0;
IfxCan_Can_initNode(&g_mcmcan.canDstNode, &g_mcmcan.canNodeConfig);
/* ==========================================================================================
* CAN filter configuration and initialization:
* ==========================================================================================
* - filter configuration is stored under the filter element number 0
* - store received frame in a dedicated RX Buffer
* - define the same message ID as defined for the TX message
* - assign the filter to the dedicated RX Buffer (RxBuffer0 in this case)
*
* - initialize the standard filter with the modified configuration
* ==========================================================================================
*/
g_mcmcan.canFilter.number = 0;
g_mcmcan.canFilter.elementConfiguration = IfxCan_FilterElementConfiguration_storeInRxBuffer;
g_mcmcan.canFilter.id1 = CAN_MESSAGE_ID;
g_mcmcan.canFilter.rxBufferOffset = IfxCan_RxBufferId_0;
IfxCan_Can_setStandardFilter(&g_mcmcan.canDstNode, &g_mcmcan.canFilter);
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
(1)In your code, TX ID0 =0x1234567, txData[0]=0x98BADCFE; txData[1]=0x10325476 Please check if above packet is transmitted.
(2)In your code, please set a breakpoint in canIsrRxHandler(), to check rxMsg.messageId if properly received, if yes, then check if it equals to RX_ID1/RX_ID2/RX_ID3, and STEP IN using debugger to check what content received from CAN bus.