- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello ,
dear experts,
The Aurix Evt board is KIT_A2G_TC367_5V_TFT. Workding environment is Aurix Development Studio V1.5
A TC367 project which works fine before.
After the reset section is moved from default 0x80000000 to 0x80020000 like below
An error is reported when try to start the mini winger debugger
After I restore the LCF_STARTPTR_CPU0 and LCF_STARTPTR_NC_CPU0 to default value 0x80000000 (given by Aurix Design Studio), the SW can work fine again.
I guess the reason is the BMHD is not point to address 0x8002000 ? So how to change the BMHD and flash into correct UCB?
the changed LSL file is attached for your reference. (zip format)
thansk and BR
Zhou Yi
Solved! Go to Solution.
- Labels:
-
AURIX
-
ispn:27401:1:0
-
l1:314:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello dw:
thank you very much. The issue was fixed after building the project in ADS V1.8
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
Hello dw:
thank you very much. The issue was fixed after building the project in ADS V1.8