TC364_EVADC
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
When using the EVADC module for voltage sampling, if I don't use SW trigger or PWM trigger, and only use GTM timer trigger, do I still need to configure interrupts? How should I choose the trigger source? Trigger 0 or Trigger 1, or others?

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/TC364-EVADC/td-p/641155

0 Likes
1 Solution
Translation_Bot
Community Manager
Community Manager
Community Manager

Hello,

You can refer to the following two programs together: you need to specify a GTM signal to start the trigger ADC. If there are relevant trigger settings, you can take a look

CCU6_ADC_1_KIT_TC375_LK

GTM_TOM_ADC_1_KIT_TC275_LK

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/TC364-EVADC/m-p/643032

View solution in original post

0 Likes
2 Replies
Translation_Bot
Community Manager
Community Manager
Community Manager

Hello,

You can refer to the following two programs together: you need to specify a GTM signal to start the trigger ADC. If there are relevant trigger settings, you can take a look

CCU6_ADC_1_KIT_TC375_LK

GTM_TOM_ADC_1_KIT_TC275_LK

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/TC364-EVADC/m-p/643032

0 Likes
Translation_Bot
Community Manager
Community Manager
Community Manager

OK thank you, I'll try

 

smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/AURIX/TC364-EVADC/m-p/643764

0 Likes