- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
The deviation is as follows:
"The simple test case of writing all 0 and checking for 1 should return a full bitmap.
However, in this device step, only one (the last) address of the SRAM is returned.
Workaround
Use the reverse test w1 - r0, which is working as expected and returns the full
bitmap."
I have trouble understanding what this errata deviation is describing. Could someone explain preferably in some examples what is the expected behavior, the actual behavior and the workaround?
Best regards
- Labels:
-
Aurix
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
The extract from Errata sheet means that if you are writing 0s and checking for 1, ideally it should return every fault in the entire test address range. But here, it is returning fault only in the last address. As a workaround, program your test memory with 1s and read 0s so that the expected result is obtained.
You can refer to this code example.
You can also refer to the section "8.4.4 Operation Modes" from tc29xB_um_v1.3 User Manual.
Regards,
Aiswarya.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
Still don't understand as it explained nothing. Writing 0 where? Checking for 1 where? Is RDBFL supposed to indicate which bits are flipped? Is this what is meant by the fail bitmap? The ETRR register should contain the fail address?
If the memory range is filled with 0x0000 and there are multiple addresses with flipped single bits to for example 0x0001, then during reading the memory range, only the last address will be contained in ETRR register? Do RDBFL registers still contain full bitmap (0x0001)? How RDBFL registers correspond to ETRR registers when there are maximum 40 and 5 of them respectively?
In case the memory is filled with 0xFFFF and there are multiple addresses with flipped single bits to for example 0xFFFE, then during reading the memory range, all of the addresses with error are contained in ETRR registers? Do RDBFL registers still contain full bitmap (0x0001)?
Best regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Writing 0 and checking for 1 in the test memory range. The fail bit map is in RDBFL and the associated address is in ETRR (0). As long as no fail has occurred RDBFL contains the last read information and ETRR has no valid data.
Kindly refer to the descriptions of MBIST Control Register, MBIST Status Register, RDBFL Register in the User Manual.
You can also refer to the Appnote given in the below link.
Also, refer to the IfxMtu_runNonDestructiveInversionTest() function in the above-mentioned code example.
Regards,
Aiswarya.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
How can you write 0 and read 1? If you write 0 then you also read 0, when you write 1 you read 1. How the expected read value is set? Is it only applicable to tests performing operations on a whole range? What about single address mode? What is contained in the RDBFL when the fail has occurred?
All of those examples describe only one use case of Non-Destructive Inversion Test with one injected error.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Any response?