Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

Not applicable
Hello,

if have a problem connecting the memtool to my Aurix TC299TX.

Connect fail always with the message:

Message from component 'IMTMemtool' :
Can't connect to Target

Message from component 'Controller0.Core0.Tc2CoreTargIntf' :
Can't connect target !

Message from component 'Controller0.Core0.Tc2CoreTargIntf' :
Can't connect JTAG target

Message from component 'Controller0.Core0.Tc2CoreTargIntf' :
Failed to read target state !


The selected controller seems to be right, because when I select an other controller I get the Error
Message from component 'Controller0.Core0.Tc2CoreTargIntf' :
That's the wrong target type !
Please check target configuration !


As JTAG device I use the miniWiggler from Infineon.
0 Likes
1 Reply
User13522
Level 1
Level 1
hello.

Have you changed BMI or Boot mode?

I had experienced to connect fail after changed BMI. ( MCU was always running in Reset mode by trip interrupt. )

Maybe You should check the DAS server whether to be right or not.

In my case, Das server was failed. so I had changed MCU.

I'm sorry i couldn't help you.

thank you.

ps. I use the Wiggler on EVB from Infineon and Device is TC234.
0 Likes