TC277: GPIO, short time max. current drive

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User21134
Level 1
Level 1
Hi all,

according to the datasheet (TC277), maximum short circuit current of a GPIOs is Isc = +-10mA.
I wonder if can drive more than 10mA for short time (less than 5 ns), which happens for example on every edge of a fast SPI clock (16MHz).

Regards, Benjamin
0 Likes
1 Reply
MoD
Employee
Employee
50 likes received 500 replies posted 100 solutions authored
Isc is the static current and can't be compared with the dynamic current in case of switching.
0 Likes