Jul 29, 2021
04:24 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jul 29, 2021
04:24 AM
hello,
. I am having a query about DMA transfer.
1) I am developing DMA driver and It requires a continous DMA transfer from Source to Destination which is intiated by Software reuest.
After going through the manual and examples I understand "CHCSR.SCH = 1" will initiate automatically DMA transfer and when i implemented in my code it doesnt work and I was getting TRAP error while debugging.
My question:- Is it possible to perform continous DMA transfer without using linked list feature?
Note:- I am using iLLD for reference.
Kindly help me on this query.
void initDMA(void)
{
// int i;
/* Load default module configuration into configuration structure */
IfxDma_Dma_initModuleConfig(&g_DMA.dmaConfig, &MODULE_DMA);
/* Initialize module with configuration. */
IfxDma_Dma_initModule(&g_DMA.dmaHandle, &g_DMA.dmaConfig);
/* Get/initialize DMA channel configuration for all DMA channels otherwise use &g_Dma.dmaChannel as target */
IfxDma_Dma_initChannelConfig(&g_DMA.dmaChNCfg, &g_DMA.dmaHandle);
/* Set desired DMA channel: Channel 0 is used */
g_DMA.dmaChNCfg.channelId = DMA_CHANNEL_ID;
/* Setup the operation mode/settings for DMA channel */
g_DMA.dmaChNCfg.moveSize = IfxDma_ChannelMoveSize_32bit;
/* Set the number of DMA transfers */
g_DMA.dmaChNCfg.transferCount = (uint16)MEMORY_TRANSFER_NUM_DATA;
/* Execute the DMA transaction with only one trigger */
g_DMA.dmaChNCfg.requestMode = IfxDma_ChannelRequestMode_completeTransactionPerRequest;
g_DMA.dmaChNCfg.shadowControl = IfxDma_ChannelShadow_srcDirectWrite;
g_DMA.dmaChNCfg.sourceAddress = (uint32)&Source;
g_DMA.dmaChNCfg.destinationAddress = (uint32)&destination;
/* Address to next TCS */
for(int i = 0; i < BUFFERSIZE ; i++){
g_DMA.dmaChNCfg.shadowAddress = (uint32)&Source[(i + 1) % BUFFERSIZE]; }
/* Enable interrupt on completion of the last DMA */
g_DMA.dmaChNCfg.channelInterruptEnabled = TRUE;
// Init DMA
IfxDma_Dma_initChannel(&g_DMA.dmaChannel, &g_DMA.dmaChNCfg);
// Autostart
g_DMA.dmaChannel.channel->CHCSR.B.SCH = 1;
/* Configure & enable DMA Channel0 interrupt */
g_dmaCh0Src_ = IfxDma_Dma_getSrcPointer(&g_DMA.dmaChannel);
IfxSrc_init(g_dmaCh0Src_, IfxSrc_Tos_cpu0, ISR_PRIORITY_DMA_CH0);
IfxSrc_enable(g_dmaCh0Src_);
}
Regards,
Deepak
. I am having a query about DMA transfer.
1) I am developing DMA driver and It requires a continous DMA transfer from Source to Destination which is intiated by Software reuest.
After going through the manual and examples I understand "CHCSR.SCH = 1" will initiate automatically DMA transfer and when i implemented in my code it doesnt work and I was getting TRAP error while debugging.
My question:- Is it possible to perform continous DMA transfer without using linked list feature?
Note:- I am using iLLD for reference.
Kindly help me on this query.
void initDMA(void)
{
// int i;
/* Load default module configuration into configuration structure */
IfxDma_Dma_initModuleConfig(&g_DMA.dmaConfig, &MODULE_DMA);
/* Initialize module with configuration. */
IfxDma_Dma_initModule(&g_DMA.dmaHandle, &g_DMA.dmaConfig);
/* Get/initialize DMA channel configuration for all DMA channels otherwise use &g_Dma.dmaChannel as target */
IfxDma_Dma_initChannelConfig(&g_DMA.dmaChNCfg, &g_DMA.dmaHandle);
/* Set desired DMA channel: Channel 0 is used */
g_DMA.dmaChNCfg.channelId = DMA_CHANNEL_ID;
/* Setup the operation mode/settings for DMA channel */
g_DMA.dmaChNCfg.moveSize = IfxDma_ChannelMoveSize_32bit;
/* Set the number of DMA transfers */
g_DMA.dmaChNCfg.transferCount = (uint16)MEMORY_TRANSFER_NUM_DATA;
/* Execute the DMA transaction with only one trigger */
g_DMA.dmaChNCfg.requestMode = IfxDma_ChannelRequestMode_completeTransactionPerRequest;
g_DMA.dmaChNCfg.shadowControl = IfxDma_ChannelShadow_srcDirectWrite;
g_DMA.dmaChNCfg.sourceAddress = (uint32)&Source;
g_DMA.dmaChNCfg.destinationAddress = (uint32)&destination;
/* Address to next TCS */
for(int i = 0; i < BUFFERSIZE ; i++){
g_DMA.dmaChNCfg.shadowAddress = (uint32)&Source[(i + 1) % BUFFERSIZE]; }
/* Enable interrupt on completion of the last DMA */
g_DMA.dmaChNCfg.channelInterruptEnabled = TRUE;
// Init DMA
IfxDma_Dma_initChannel(&g_DMA.dmaChannel, &g_DMA.dmaChNCfg);
// Autostart
g_DMA.dmaChannel.channel->CHCSR.B.SCH = 1;
/* Configure & enable DMA Channel0 interrupt */
g_dmaCh0Src_ = IfxDma_Dma_getSrcPointer(&g_DMA.dmaChannel);
IfxSrc_init(g_dmaCh0Src_, IfxSrc_Tos_cpu0, ISR_PRIORITY_DMA_CH0);
IfxSrc_enable(g_dmaCh0Src_);
}
Regards,
Deepak
- Tags:
- IFX
0 Replies