TC275芯片通过Mcal进行底层开发时,tasking编译器的话需要修改lsl哪些地方,有大神清楚吗?

公告

大中华汽车电子生态圈社区并入开发者社区- 更多资讯点击此

Tip / 登入 to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Twin
Level 5
Level 5
5 solutions authored First solution authored First like received
如题: link的时候报了这个错误,实在不懂什么情况 relocation error in "task1": relocation value 0x80008300, type abs18 space, offset 0x8, section ".text.Shared.DEFAULT_CODE_ROM" at address 0x80030894 is not a valid address in R_TRICORE_18ABS. Hint: check the mapfile for a section that occupies this address.
0 点赞
7 回复数
quentin1
Level 4
Level 4
100 replies posted 50 replies posted 25 replies posted
lsl 不要修改,Tasking编译时 要在setting-link-script中添加lsl文件路径,不同版本号的mcal添加对应版本的lsl文件。
0 点赞
meng0604010
Level 4
Level 4
50 replies posted 25 replies posted 10 replies posted
xueixile
0 点赞
lengxue1151204
Level 3
Level 3
50 replies posted 25 replies posted 10 replies posted
可以找到MCAL中提供的lsl文件,然后在此基础上进行修改
0 点赞
evenchen
Level 4
Level 4
Distributor - Intron(GC)
10 sign-ins First reply posted First like given
一般不要直接修改安装目录下的lsl文件,可以直接考到工程里面 MCAL的安装包里面有lsl的修改参考工程 C:EB resos27X_DCMC-ISAR_AS4XX_AURIX_TC27X_DC_PB_BASE_V500_REL322TC27x_DCstepAurix_MC-ISAR
0 点赞
天河之外
Level 5
Level 5
100 replies posted 50 replies posted 25 replies posted
学习一下
0 点赞
SIX_66
Level 6
Level 6
First comment on blog 500 replies posted 250 replies posted
学习学习
0 点赞
撸起袖子
Level 1
Level 1
Welcome! 5 replies posted First question asked
请问最后这个问题怎么解决的?
0 点赞