TC234LP32F200NACKXUMA1 Security Features

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User19684
Level 1
Level 1
10 replies posted 5 replies posted First question asked
Hello Support Team,
-Can you provide me with the type of Evita for this part number TC234LP32F200NACKXUMA1. IS it Full HSM or Medium HSM?
-Also can you provide me if this part number support SHE HIS security standards?
-Also is this part number Supports AutoSAR technology? and If yes what is its version and what is its availability date?
-Is there safety documents/Manual studies related to this product?

Thanks
Ahmed Sabry
0 Likes
10 Replies
cwunder
Employee
Employee
100 solutions authored 5 likes given 50 likes received
- This device is Medium Evita (since it doesn't have an asymmetric HW Crypto Engine), TC3xx supports full Evita
- SHE HIS is realized with software that runs on the HSM, TC234LP the "P" indicates it has an HSM
- AUTOSAR solutions are available for this device you need to contact your Infineon representative for further information.
- Safety documentation and Manual requires you to contact your Infineon representative.
0 Likes
User19684
Level 1
Level 1
10 replies posted 5 replies posted First question asked
Can I consider each device which has HSM to be SHE HIS as a general concept?
0 Likes
cwunder
Employee
Employee
100 solutions authored 5 likes given 50 likes received
The HSM has the hardware features for the SHE, it depends on the software implementation to realize the functionality along with how you use the Data Flash for the Key management. You should discuss this with your Infineon representative as they also use third party security vendors for HSM.
0 Likes
User19684
Level 1
Level 1
10 replies posted 5 replies posted First question asked
Thank you for your support, can you help if available to detect the type of EVITA : Full HSM or Medium HSM or Light HSM for the below Infineon Families?
XC866 TC234L XC2238N24F40 XC2298H200F100 XC2388C
TC1796 TC275TP64F200 XC2238N40 XC2299H200F100 XC2388E136F128
TC1762 SAK-TC277T-64F XC2263N XC2336A XC2734X
TC1766 TC1782 SAK-XC2265N-40 XC2336B XC2764X
XC2786X XC2234L20F66 XC2265N40F80 XC2336B40F66LAAKXUMA1 XC2765X10
XC2387A SAK-XC2236N-40 XC2267M104F XC2336B40 TC297TP128F300
TC1767 TC1724 SAK-XC2267M XC2361A56F80 TC297TX128F300
TC1736 TC1791 XC2267M72 XC2361A72F80 TC297TA128
XC2766X SAK-TC1793 XC2268I136F128LAA XC2361B40 TC299T128F300
TC233LP32F200 TC1793F512F270 SAK-XC2268I XC2361B40F XC2785X10
TC1728 SAK-TC1797-512F180 XC2268N40 XC2361E136F128 TC299TX
TC1736 TC1197 XC2269I136F128 XC2364A10
TC1762 TC1798 XC2287M10 XC2364B40F80
TC1796256F XC2237M104F80L XC2287M72F80 XC2365A10
XC836MT2FR TC297TP128 XC2288H200F100 XC2365A72F80
C164 TC277TP64F200 XC2289H200 XC2365B40F80
TC1766 TC297TX128 XC2289I136F128L XC2368E
0 Likes
User19684
Level 1
Level 1
10 replies posted 5 replies posted First question asked
can you help detect the type of EVITA : Full HSM or Medium HSM or Light HSM for the below Infineon Families and if these parts are supported by SHE HIS or not?

ADSP-BF532SBST400
TC233LP32F200NACKXUMA1
SAF-XC866-4FRI BE
SAK-TC1728N-192F133HL
TC1736128F80HLAAKXQMA1
TC1762128F66HLACKXUMA4
ADUCM331WDCPZ-U10
SAK-TC1762-128F80HL AC
SAK-TC1796-256F150E
TC90400FG
EPM2210F256A5N
TMS320DA150PGE160
CT80618003201ABSLJ38
DRA722AHGABCQ1
SAK-XC836MT-2FRA AB
DRA722AHGABCRQ1
TMS320DM642AZDKA5
TMS320F2812GHHQR
MB86R02PBH-GSE1
MB86R12FBH-GSE1

I appreciate your help urgently.
0 Likes
User19684
Level 1
Level 1
10 replies posted 5 replies posted First question asked
can you help detect the type of EVITA : Full HSM or Medium HSM or Light HSM for the below Infineon Families and if these parts are supported by SHE HIS or not?

ADSP-BF532SBST400
TC233LP32F200NACKXUMA1
SAF-XC866-4FRI BE
SAK-TC1728N-192F133HL
TC1736128F80HLAAKXQMA1
TC1762128F66HLACKXUMA4
ADUCM331WDCPZ-U10
SAK-TC1762-128F80HL AC
SAK-TC1796-256F150E
TC90400FG
EPM2210F256A5N
TMS320DA150PGE160
CT80618003201ABSLJ38
DRA722AHGABCQ1
SAK-XC836MT-2FRA AB
DRA722AHGABCRQ1
TMS320DM642AZDKA5
TMS320F2812GHHQR
MB86R02PBH-GSE1
MB86R12FBH-GSE1
0 Likes
NeMa_4793301
Level 6
Level 6
10 likes received 10 solutions authored 5 solutions authored
A lot of those aren't Infineon parts 😉

Only the TC233 is recommended for long-term designs, and it supports EVITA Medium. The AURIX HSM is programmable and requires software from Escrypt, Vector, Elektrobit, or Green Hills Integrity to implement SHE functionality.

The TC17xx and XC8xx parts may be phased out after 2024.
0 Likes
User19684
Level 1
Level 1
10 replies posted 5 replies posted First question asked
can you help detect the type of EVITA : Full HSM or Medium HSM or Light HSM for the below Infineon Families and if these parts are supported by SHE HIS or not?
I need this information even if these parts are obsolete or not recommended for new design:
SLI 76CF5120P >>> http://download.siliconexpert.com/pdfs2/2019/3/6/18/36/6/528877/smn_/manual/44444444gies.pdf
XC866 >>> http://download.siliconexpert.com/pdfs/2007/11/28/semi_ap/manual/smn/ds/xc866_ds_v12.pdf
TC1728 >>> http://download.siliconexpert.com/pdfs/2012/5/31/2/55/53/3/smn_/manual/tc1728_ds_v1_0.pdf
TC1736 >>> http://download.siliconexpert.com/pdfs/2009/12/16/18/6/36/934/smn_/auto/tc1736_ds_v1.1.pdffolderiddb...
TC1762 >>> http://download.siliconexpert.com/pdfs/2008/05/03/semi_ap/manual/smn/microcontroller/tc1762_ds_v10.p...
TC1796256F >>> http://download.siliconexpert.com/pdfs/2008/04/27/semi_ap/manual/smn/microcontroller/tc1796_ds_v1.0....
XC836MT2FR >>> http://download.siliconexpert.com/pdfs/2011/10/16/1/15/23/43/smn_/manual/xc835_xc836_ds_v1.1d2.pdf
C164 >>> http://download.siliconexpert.com/pdfs/mcu/smn/c164ci_ds_v2.0_2001_05_15.pdf
TC1766-192F >>> http://download.siliconexpert.com/pdfs/2008/05/03/semi_ap/manual/smn/microcontroller/tc1766_ds_v10.p...
TC234L >>> http://download.siliconexpert.com/pdfs2/2019/3/16/2/16/44/883559/smn_/manual/infineon-tc23xl-aurix_f...
TC1767 >>> http://download.siliconexpert.com/pdfs/2009/12/16/18/28/5/411/smn_/auto/tc1767_product_brief.pdffold...
TC270TP >>> http://download.siliconexpert.com/pdfs/2015/11/22/1/25/20/484/smn_/manual/epn_03783aerra_1448036105....
TC275TP64F200 >>> http://download.siliconexpert.com/pdfs/2018/1/2/6/27/58/579/smn_/manual/pgurl_tc275tp64f200ndckxuma1...
TC277T-64F >>> http://download.siliconexpert.com/pdfs/2013/7/21/1/30/18/468/smn_/manual/tc27xtsafety.pdf
XC2285M >>> http://download.siliconexpert.com/pdfs/2011/8/10/0/35/18/510/smn_/manual/xc228xm_ds_v2.0_2009_03.pdf
XC2387A >>> http://download.siliconexpert.com/pdfs/2009/12/16/18/2/14/698/smn_/auto/xc2387a_pb.pdffolderiddb3a30...
XC2387E >>> http://download.siliconexpert.com/pdfs/2016/1/26/3/9/50/796/smn_/manual/929infineon-xc238xe-ds-v01_0...
TC1782 >>> http://download.siliconexpert.com/pdfs/2014/6/8/1/31/27/226/smn_/manual/9748tc1782_ds_v141.pdffolder...

Appreciate your fast response.
0 Likes
Harvey
Employee
Employee
XC8xx and XC2xx are not support any HW feature for security
In case of 8-bit and 16-bit MCUs, there is not HW feature for security.

From TC17xx, Infineon 32-bit MCU can support HW feature for security

TC1791/93/98 is HIS compliant.
TC23x/TC27x/TC29x are HIS compliant and Medium Evita
TC3xx is HIS compliant and Full Evita

Nowadays, in case of new projects, TC3xx is preferred because of Full Evita support.
0 Likes
Harvey
Employee
Employee
XC8xx and XC2xx are not supported any HW feature for security
In case of 8-bit and 16-bit MCUs, there is not HW feature for security.

From TC17xx, Infineon 32-bit MCU can support HW feature for security

TC1791/93/98 is HIS compliant.
TC23x/TC27x/TC29x are HIS compliant and Medium Evita
TC3xx is HIS compliant and Full Evita

Nowadays, in case of new projects, TC3xx is preferred because of Full Evita support.
0 Likes