Aug 19, 2020
05:06 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Aug 19, 2020
05:06 AM
Hi,
As title says, BIV is empty (0x0).
Interrupt is not being generated. Currently using iLLD_1_0_1_11_0 with hightec toolchain.
How do I update vector table?
Code is as follows.
As title says, BIV is empty (0x0).
Interrupt is not being generated. Currently using iLLD_1_0_1_11_0 with hightec toolchain.
How do I update vector table?
Code is as follows.
// Module Header
#include "Cpu0_Main.h"
#include
#include
#include "../hsi_misc/IfxCpu.h"
#include "../hsi_misc/IfxScu_reg.h"
#include "../hsi_misc/IfxAsclin.h"
#include "../hsi_misc/IfxDts_Dts.h"
#include "../hsi_misc/IfxStm.h"
#include "../hsi_misc/Bsp.h"
#include "../hsi_misc/IfxScuWdt.h"
#include "../hsi_misc/IfxGpt12.h"
#define SPB_FREQ PLL_FREQUENCY/2
#define PLL_FREQUENCY 200000000.0f
IfxStm_CompareConfig g_STMConf; /* STM configuration structure */
void initSTM(void);
void Gpt12_T3_ISRHandler(void);
IFX_INTERRUPT(isrSTM, 0, ISR_PRIORITY_STM0);
// void __interrupt(ISR_PRIORITY_STM0) isrSTM(void);
IFX_INTERRUPT(Gpt12_T3_ISRHandler, 0, ISR_PRIORITY_T3);
void isrSTM(void)
{
/* Update the compare register value that will trigger the next interrupt and toggle the LED */
IfxStm_increaseCompare(&MODULE_STM0, g_STMConf.comparator, IfxStm_getTicksFromMicroseconds(&MODULE_STM0,1000u));
while(1) {;}
}
void Gpt12_T3_ISRHandler(void)
{
while(1) {;}
}
int main(void)
{
// __mtcr(CPU_BIV, (uint32)__INTTAB_CPU(0));
// Change watchdog timer value before timeout
IfxScuWdt_changeCpuWatchdogReload(IfxScuWdt_getSafetyWatchdogPassword(),0xff00);
// Disable the watchdog timers
IfxScuWdt_disableCpuWatchdog(IfxScuWdt_getCpuWatchdogPassword());
IfxScuWdt_disableSafetyWatchdog(IfxScuWdt_getSafetyWatchdogPassword());
IfxScuCcu_Config clocks;
IfxScuCcu_initConfig(&clocks);
// Configure the PLL dividers
IfxScuCcu_calculateSysPllDividers(&clocks,PLL_FREQUENCY);
// Initialise CCU
IfxScuCcu_init(&clocks);
// Set SPB frequency
IfxScuCcu_setSpbFrequency(PLL_FREQUENCY/4); // 50 Mhz
// IfxCpu_enableInterrupts(); // Disab
IfxStm_initCompareConfig(&g_STMConf); /* Initialize the configuration structure with default values */
g_STMConf.triggerPriority = ISR_PRIORITY_STM0; /* Set the priority of the interrupt */
g_STMConf.typeOfService = IfxSrc_Tos_cpu0; /* Set the service provider for the interrupts */
g_STMConf.ticks = IfxStm_getTicksFromMicroseconds(&MODULE_STM0,1000u); /* Set the number of ticks after which the timer triggers an
* interrupt for the first time */
IfxStm_initCompare(&MODULE_STM0, &g_STMConf); /* Initialize the STM with the user configuration */
// Init the GPT12 module
IfxGpt12_enableModule(&MODULE_GPT120);
IfxGpt12_T3_run(&MODULE_GPT120, IfxGpt12_TimerRun_stop); //stop the timer just in case fixme
IfxGpt12_setGpt1BlockPrescaler(&MODULE_GPT120,IfxGpt12_Gpt1BlockPrescaler_4);
// Init T3 Timer
IfxGpt12_T3_setMode(&MODULE_GPT120, IfxGpt12_Mode_timer); // Set Timer3 to timer mode
IfxGpt12_T3_setTimerDirection(&MODULE_GPT120, IfxGpt12_TimerDirection_down);
IfxGpt12_T3_setTimerPrescaler(&MODULE_GPT120, IfxGpt12_TimerInputPrescaler_8);
IfxGpt12_T3_setTimerValue(&MODULE_GPT120, 0XFF00); // To load in Monittor_start();
// Init the T3 interrupt
volatile Ifx_SRC_SRCR *source_address = IfxGpt12_T3_getSrc(&MODULE_GPT120); // Interrupt address
IfxSrc_init(source_address, ISR_PROVIDER(INTERRUPT_T3), ISR_PRIORITY(INTERRUPT_T3)); // Init service request(CPU0..2)
IfxSrc_enable(source_address);
IfxCpu_resetAndStartCounters(IfxCpu_CounterMode_normal);
float T3_frequency = IfxGpt12_T3_getFrequency(&MODULE_GPT120);
unsigned int reload_value = (uint16)((T3_frequency/1000000)*(500));
IfxGpt12_T3_setTimerValue(&MODULE_GPT120,reload_value);
IfxGpt12_T3_run(&MODULE_GPT120, IfxGpt12_TimerRun_start);
// __enable();
while (TRUE)
{
REGRESSION_RUN_STOP_PASS;
}
return 0;
}
- Tags:
- IFX
4 Replies
Aug 19, 2020
09:44 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Aug 19, 2020
09:44 AM
In the cstart file you should see a line like
This will load the BIV register with the base address for the interrupt vector table for that CPU.
/* Load Base Address of Interrupt Vector Table. we will do this later in the program */
__mtcr(CPU_BIV, (uint32)__INTTAB(0));
This will load the BIV register with the base address for the interrupt vector table for that CPU.
Aug 19, 2020
09:47 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Aug 19, 2020
09:47 AM
Hi Fernandes. This is normally part of the Base Project template - see 0_Src\BaseSw\Infra\ssw\tc39b\Tricore\ifx_ssw_tc0.c:
Did you follow the steps described in the Hightec app note to create your project?
https://free-entry-toolchain.hightec-rt.com/HighTec_Free_TriCore_Entry_Toolchain_Migration_Guide.pdf
You might also consider using the relatively new AURIX Development Studio.
static void __Core0_start(void)
{
/* Update safety and cpu/safety watchdog reload values */
/* Password value is read again, because there is chance that local variables may be overridden. */
unsigned short cpuWdtPassword = Ifx_Ssw_getCpuWatchdogPasswordInline(&MODULE_SCU.WDTCPU[0]);
unsigned short safetyWdtPassword = Ifx_Ssw_getSafetyWatchdogPasswordInline();
Ifx_Ssw_clearCpuEndinitInline(&MODULE_SCU.WDTCPU[0], cpuWdtPassword);
// other stuff
/* Set A0 Pointer to access global variables with small data addressing */
Ifx_Ssw_setAddressReg(a0, __SDATA1(0));
/* These to be un commented if A8 and A9 are required to be initialized */
Ifx_Ssw_setAddressReg(a8, __SDATA3(0));
Ifx_Ssw_setAddressReg(a9, __SDATA4(0));
/* Trap vector table initialization is necessary if it is not same as default value */
Ifx_Ssw_MTCR(CPU_BTV, (unsigned int)__TRAPTAB(0));
/* Base interrupt vector table initialized */
Ifx_Ssw_MTCR(CPU_BIV, (unsigned int)__INTTAB(0));
/* Interrupt stack pointer is configured */
Ifx_Ssw_MTCR(CPU_ISP, (unsigned int)__ISTACK(0));
Did you follow the steps described in the Hightec app note to create your project?
https://free-entry-toolchain.hightec-rt.com/HighTec_Free_TriCore_Entry_Toolchain_Migration_Guide.pdf
You might also consider using the relatively new AURIX Development Studio.
Aug 20, 2020
02:02 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Aug 20, 2020
02:02 AM
Did you follow the steps described in the Hightec app note to create your project?
https://free-entry-toolchain.hightec...tion_Guide.pdf
I tried this but the link to BIFACES is broken. Infineon returns with "Server: sso.infineon.com
Unable to authenticate the user."
I am accustomed to Hightec now and would like to continue using it.
The __INTTAB_CPU funtion seems to be undefined although the compiler file contains :
extern unsigned int __USTACK##cpu[]; /**< user stack end */ \
extern unsigned int __ISTACK##cpu[]; /**< interrupt stack end */ \
extern unsigned int __INTTAB_CPU##cpu[]; /**< Interrupt vector table */ \
extern unsigned int __TRAPTAB_CPU##cpu[]; /**< trap table */ \
extern unsigned int __CSA##cpu[]; /**< context save area 1 begin */ \
extern unsigned int __CSA##cpu##_END[]; /**< context save area 1 begin */
#define __USTACK(cpu) __USTACK##cpu
#define __ISTACK(cpu) __ISTACK##cpu
#define __INTTAB_CPU(cpu) __INTTAB_CPU##cpu
#define __TRAPTAB_CPU(cpu) __TRAPTAB_CPU##cpu
#define __CSA(cpu) __CSA##cpu
#define __CSA_END(cpu) __CSA##cpu##_END
/*Wrapper macros for the tool specific definitions */
#if defined(IFX_USE_SW_MANAGED_INT)
#define __INTTAB(cpu) ((unsigned int)__INTTAB_CPU##cpu | (unsigned int)0x1FE0)
#else
#define __INTTAB(cpu) __INTTAB_CPU##cpu
#endif /*defined(IFX_USE_SW_MANAGED_INT) */
#define __TRAPTAB(cpu) __TRAPTAB_CPU##cpu
#define __SDATA1(cpu) __A0_MEM
#define __SDATA2(cpu) __A1_MEM
#define __SDATA3(cpu) __A8_MEM
#define __SDATA4(cpu) __A9_MEM
The startup file my program uses is the crt0-tc2x.S and the start codes are as follows:
_start:
.code32
j _startaddr
.align 2
_startaddr:
mfcr %d0,CORE_ID # core ID
and %d1,%d0,7 # CORE_ID_MASK
sh %d2,%d1,3 #* 8
sh %d1,%d1,2 #* 4
add %d2,%d2,%d1 # offset for SCU_WDTCPUnCON0 reg =* 12
movh.a %a2,hi:SCU_WDTCPU0CON0
lea %a2,[%a2]lo:SCU_WDTCPU0CON0
mov.a %a7,%d2
add.a %a7,%a2,%a7 # addr of SCU_WDTCPUnCON0
do_endinit_cpuN:
ld.w %d1,[%a7]0 # %d1 = *SCU_WDTCPUnCON0
jz.t %d1,1,endinit_done_cpuN # einit is cleared, set it
mov.aa %a4,%a7
jl asm_set_endinit_xx # %a4 is set to SCU_WDTCPUnCON0
endinit_done_cpuN:
mfcr %d0,CORE_ID # core ID
jz %d0,do_endinit_s # Safety WDT handled by CPU0
j init_stack_pointers
do_endinit_s:
movh.a %a4,hi:SCU_WDTSCON0
lea %a4,[%a4]lo:SCU_WDTSCON0
ld.w %d1,[%a4]0 # %d1 = *SCU_WDTSCON0
jz.t %d1,1,endinit_done_s # einit is cleared, set it
jl asm_set_endinit_xx # %a4 is set to SCU_WDTSCON0
endinit_done_s:
movh.a %a4,hi:SCU_WDTCPU0CON0
lea %a4,[%a4]lo:SCU_WDTCPU0CON0
jl asm_clear_endinit_xx # %a4 is set to cpu0
init_stack_pointers:
/*
* initialize user and interrupt stack pointers
*/
movh.a %sp,hi:__USTACK # load %sp
lea %sp,[%sp]lo:__USTACK
movh %d0,hi:__ISTACK # load $isp
addi %d0,%d0,lo:__ISTACK
mtcr $isp,%d0
isync
Sep 07, 2020
04:07 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Sep 07, 2020
04:07 AM
Resolved successfully using different linker file