Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

User13360
Level 1
Level 1
Hi All,

I'm trying to figure out if this is possible

TC1796 Connecting with Memtool and Miniwiggler via CAN

Since the UCAN interface can't be had anymore, can I just add a CAN Transceiver to the Miniwiggler3 ? I see oin 18=TGIRXD and 20=USER0TXD of the Auto20 connector

See AP56004


How can I use this to do CAN Bootloader with Memtool ?

I appreciate your thoughts

Best Regards,

Rapid
0 Likes
3 Replies
MoD
Employee
Employee
250 sign-ins 25 likes received 50 solutions authored
Hi,
This will not be possible. The miniWiggler can't be use to access the device via CAN bootstrap loaeder. Everything described in the pdf about CAN is for using an external frontend for DAP over CAN if the connected device support this. TC1796 don't support DAP also not DAP over CAN.
0 Likes
User13360
Level 1
Level 1
Thanks MoD for your reply
0 Likes
User21944
Level 1
Level 1
Hi All,
Where can I buy an “external frontend for DAP over CAN" for the "MiniWiggler V3 USB".
If no frontend is available a schematic or some detailed description would be very helpful!
Thanks
Holger
0 Likes
This widget could not be displayed.