Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

pistons7
Level 3
Level 3
50 sign-ins 5 likes given First solution authored

The Port-14.1 is set as CAN reception port.

I want to detect CAN reception using the WCAN interrupt on the SCR side, but it doesn't work.

The WCAN settings for the SCR are as follows.
What is the problem?

The CAN ID being sent is 10200101h.
Communication speed is 250k.

/* WCAN Start */
SCR_SCU_PAGE = 2;
SCR_MODPISEL0 = 0x50; // WCANRXDF

SCR_WCAN_PAGE = 0;
SCR_WCAN_CFG = SCR_WCAN_CFG | 0x01; // WCAN_EN = 1
SCR_WCAN_CFG = SCR_WCAN_CFG | 0x08; // CCE = 1
SCR_IEN1 = SCR_IEN1 | 0x01;/* Enable WCAN filter interrupts */


//configure baud rate
SCR_WCAN_PAGE = 1;
SCR_WCAN_BTL1_CTRL = 0x64;
SCR_WCAN_BTL2_CTRL = SCR_WCAN_BTL2_CTRL & 0x3F;
SCR_WCAN_BTL2_CTRL = SCR_WCAN_BTL2_CTRL | 0xC0;

// CDR setting
SCR_WCAN_PAGE = 0;
SCR_WCAN_CDR_CTRL = SCR_WCAN_CDR_CTRL & 0xFE;
SCR_WCAN_CDR_CTRL = SCR_WCAN_CDR_CTRL | 0x01; //Enable CDR


SCR_WCAN_PAGE = 0;
SCR_WCAN_CFG = SCR_WCAN_CFG & 0xF7; // CCE = 0
SCR_WCAN_CFG = SCR_WCAN_CFG & 0xFB; // SELWK_EN = 0
SCR_WCAN_INTMRSLT = 0x0F;

SCR_WCAN_PAGE = 0;
SCR_WCAN_CFG = SCR_WCAN_CFG | 0x04; // SELWK_EN = 1

// SCR_WCAN_PAGE = 1;
while( !( SCR_WCAN_INTESTAT0 & 0x01) )
{
}

SCR_WCAN_PAGE = 1;
SCR_WCAN_DLC_CTRL = 0x08; //DLC = 8

SCR_WCAN_PAGE = 2;
SCR_WCAN_ID0_CTRL = 0xFF;
SCR_WCAN_ID1_CTRL = 0xFF;
SCR_WCAN_ID2_CTRL = 0xFF;
SCR_WCAN_ID3_CTRL = 0x10;

SCR_WCAN_MASK_ID0_CTRL = 0x00;
SCR_WCAN_MASK_ID1_CTRL = 0x00;
SCR_WCAN_MASK_ID2_CTRL = 0x00;
SCR_WCAN_MASK_ID3_CTRL = 0x00;

SCR_WCAN_PAGE = 0;
SCR_WCAN_CFG = SCR_WCAN_CFG & 0xFB;
SCR_WCAN_CFG = SCR_WCAN_CFG | 0x04; //SELWK_EN = 1b

SCR_WCAN_INTMRSLT = 0x0C; //Wake-Up CAN Interrupt Mask Register

// SCR_WCAN_PAGE = 1;
while( ( SCR_WCAN_INTESTAT0 & 0x01 ) != 1 )
{
}


/* WCAN End */

0 Likes
2 Replies
dw
Moderator
Moderator
Moderator
1000 replies posted 250 solutions authored 100 likes received

9999999.png

Could you please check if this code is useful?

0 Likes
dw
Moderator
Moderator
Moderator
1000 replies posted 250 solutions authored 100 likes received

SWKSET = 1 only when:

• WCAN_CFG.WCAN_EN = 1b
• WCAN_CFG.CCE = 0b -->
• WCAN_INTESTAT0.SWACK = 1b
• WCAN_INTESTAT0.MODE = 0b

 

This bit getting set in the code WCAN_CFG.WCAN_EN. 

1. Reset the bit  WCAN_CFG.SELWK_EN 

2. Wait until WCAN_INTESTAT0.SWACK =0

3. //WUF register to be configured 

4. Set WCAN_CFG.SELWK_EN = 1b

5. Wait until WCAN_INTESTAT0.SWACK = 1b

0 Likes
This widget could not be displayed.