Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

User19757
Level 1
Level 1
Hi,

I just installed AURIX Studio Ver. 1.1.10.

I tried to create a new project, but I can't find the TC37x series in the device list.
(From what I've seen, only up to the TC2xx is available.)

Can you tell me where to find a sample code for TC37x?
0 Likes
5 Replies
NeMa_4793301
Level 6
Level 6
10 likes received 10 solutions authored 5 solutions authored
AURIX Development Studio doesn't support TC3xx yet - but it should by the end of July.
0 Likes
User19757
Level 1
Level 1
Thank you.
I understand that it is unsupported.

I'm sorry for the additional questions.

There are evaluation boards such as "KIT_A2G_TC3**" on the market.
Isn't there sample code available for evaluation using these as well?
(Do I have to code the header files and startups myself?)
0 Likes
MoD
Employee
Employee
250 sign-ins 25 likes received 50 solutions authored
0 Likes
User19757
Level 1
Level 1
Dear Mod.

Thanks for your answer.

However, when I open the link, it says "Unable to authenticate the user." It was and I couldn't get to the end of the link.
(I can log in to "infineon.com", so it's not a typing error. )

I'm aware that the TC2xx code is available on GitHub, but it's not published in TC3xx as well, am I correct?
(TC3xx is currently unsupported, so at best it's just a distribution of drivers, etc.?)
https://github.com/Infineon/AURIX_code_ examples
0 Likes
User19757
Level 1
Level 1
Sorry. I was mistaken.
I was able to get the set from the URL using an account with access rights.

Thank you for your help.
0 Likes