Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

User16740
Level 1
Level 1
5 replies posted 5 questions asked First reply posted
The SafeTLib (535) has been configured and built for proprietary TC275 based hardware.

There are 56 tests in total, distributed over all three cores. The only test not run is Lockstep on core 1, as it's not currently enabled (Not my decision, don't ask).

All tests are passing, apart from the Input Output Monitor (IOM) Test, which reports a 0x221502 (IOMTST_ALARMNOTSETERR).

I have:

  • Read the SafeTLib User Manual IOM test section at least five times.
  • Ensured that the AoU are met (22K pull-down).
  • Debugged the test and checked that the pin read back state toggles.
  • Removed the 22K pull down.
  • Tried the test on all three cores.
  • Tried different pins.
  • Tried different LAMs.
  • Checked the Release Notes.
  • Checked the Addendum.
  • Compared with existing projects.


I can't get this one test to pass, does anyone have any idea what I'm doing wrong?
0 Likes
2 Replies
NeMa_4793301
Level 6
Level 6
10 likes received 10 solutions authored 5 solutions authored
A 22K pull-down conflicts with this part of the Release Notes Addendum:
GPIO pin used for IomTst shall not be connected to external circuitry which forces the pin to a permanent high/low state during the test

With a 22K pull-down vs. the weak internal pull devices, it might have taken a few more clock cycles to reach a high state. It might look okay in the debugger, but at full speed, it might not work.

Have you tried it on a pin that's simply open? Which pin and LAM are you using?
0 Likes
User16740
Level 1
Level 1
5 replies posted 5 questions asked First reply posted
I asked a hardware engineer to physically remove the resistor from the PCB and now the test is passing.

Thanks.
0 Likes
This widget could not be displayed.