- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello. Infienon team
here are my 2 question.
Q1.
I'm using TC364DP MCU and also using TLE5012B Motor position sensor.
I'm trying to communicate with SSC protocol, it doesn't workl well.
And i'm using ILLD example code, but i can't find SSC example in ILLD.
i think MPS and MCU are both infineon product, so i think there is sample code.
can you give sample code? help me.
Q2.
If you doesn't have TLE5012's ILLD code or sample code, i have anther question.
I implemented communication via QSPI ILLD module.
But SSC's protocol is different to SPI communication, so i can't get exact data.
i want to know how QSPI module works.
here is my question.
If QSPI module's RX pin get data and RX buffer is filled, then RX ISR is called even though QSPI module doesn't work?
the topology is below picture. MCU's MOSI and MISO is connected to same node(P6111) .
so, when i try to communicate via ILLD QSPI module, my sending command is returned via nodeP6111. i don't know how to implement via ILLD QSPI module.
can you help me to implement SSC communication via QSPI ILLD module?
thank you.
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
Hello. dw.
i have more question about QSPI module usage method by using ILLD.
i think i can implement SSC communication by using QSPI module. here is my method.
1. set QSPI module as Tx mode, and disable Rx pin and send command
2.change QSMPI module as Rx mode(set Tx pin as Rx or disable Tx pin and just using Rx pin
3. get data
so, i made samle code, but it isnt' work when i assign Rx pin or Tx pin as NULL_PTR.
I understand that there are fixed pins that I can use for QSPI Tx and Rx. However, all of these pins are already in use, so I cannot allocate them. Therefore, I allocated NULL_PTR to unused pins. However, if I use this method, the program stops in the IfxQspi_SpiMaster_exchange function.
here is my question.
How can I use the QSPI module exclusively for MOSI (Tx) and MISO (Rx)? Can you provide an example code? The following code is my example code, but it is not working properly. I would like to inquire about what went wrong.
The function in the following code aims to convert the QSPI module between Tx mode and Rx mode.
void tx_QSPI1_Master(void)
{
/* QSPI1 */
IfxQspi_SpiMaster_initModuleConfig(&spiMasterConfig[1], &MODULE_QSPI1); /* Initialize it with default values */
spiMasterConfig[1].base.mode = SpiIf_Mode_master;
spiMasterConfig[1].base.maximumBaudrate = 4000000;
// qspi1_m_init_pins();
// IfxPort_setPinMode(&MODULE_P10, 1,IfxPort_Mode_outputPushPullAlt2);
const IfxQspi_SpiMaster_Pins qspi1_pins = {
&IfxQspi1_SCLK_P10_2_OUT, IfxPort_OutputMode_pushPull, /* SCLK Pin (CLK) */
&IfxQspi1_MTSR_P10_3_OUT, IfxPort_OutputMode_pushPull, /* Master Transmit Slave Receive Pin (MOSI) */
NULL_PTR, IfxPort_InputMode_pullDown, /* Master Receive Slave Transmit Pin (MISO) */
0 /* Pad driver mode */
};
spiMasterConfig[1].pins = &qspi1_pins; /* Assign Master Pins */
spiMasterConfig[1].base.txPriority = ISR_PRIORITY_QSPI1_TX;
spiMasterConfig[1].base.rxPriority = ISR_PRIORITY_QSPI1_RX;
spiMasterConfig[1].base.erPriority = ISR_PRIORITY_QSPI1_ER;
spiMasterConfig[1].base.isrProvider = IfxSrc_Tos_cpu0;
/* Initialize the QSPI Master module using the user configuration */
IfxQspi_SpiMaster_initModule(&g_spiMaster[1], &spiMasterConfig[1]);
}
void rx_QSPI1_Master(void)
{
/* QSPI1 */
IfxQspi_SpiMaster_initModuleConfig(&spiMasterConfig[1], &MODULE_QSPI1); /* Initialize it with default values */
spiMasterConfig[1].base.mode = SpiIf_Mode_master;
spiMasterConfig[1].base.maximumBaudrate = 4000000;
// qspi1_m_init_pins_rx();//set port as output pin
// IfxPort_setPinMode(&MODULE_P10, 1, IfxPort_Mode_inputPullUp);
const IfxQspi_SpiMaster_Pins qspi1_pins = {
&IfxQspi1_SCLK_P10_2_OUT, IfxPort_OutputMode_pushPull, /* SCLK Pin (CLK) */
NULL_PTR, IfxPort_InputMode_pullDown, /* Master Transmit Slave Receive Pin (MOSI) */
&IfxQspi1_MRSTA_P10_1_IN, IfxPort_InputMode_pullDown, /* Master Receive Slave Transmit Pin (MISO) */
0 /* Pad driver mode */
};
spiMasterConfig[1].pins = &qspi1_pins; /* Assign Master Pins */
spiMasterConfig[1].base.txPriority = ISR_PRIORITY_QSPI1_TX;
spiMasterConfig[1].base.rxPriority = ISR_PRIORITY_QSPI1_RX;
spiMasterConfig[1].base.erPriority = ISR_PRIORITY_QSPI1_ER;
spiMasterConfig[1].base.isrProvider = IfxSrc_Tos_cpu0;
/* Initialize the QSPI Master module using the user configuration */
IfxQspi_SpiMaster_initModule(&g_spiMaster[1], &spiMasterConfig[1]);
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Please first refer to this SPI example code, if you make it work, then migrate to P10.2/3.
Tx and Rx can be enabled together, just to set a flag TX_DONE, if the flag is set , then Rx interrupt is enabled. The procedure is like below:
Send Data
Enable Rx INT
Receive Data
Disable Rx INT
Send Data
...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello. i tried above method, and it still doesn't works.
i made flag and add it to interrupt function.
/* QSPI1 ISR */
void qspi1_Tx_ISR(void)
{
IfxCpu_enableInterrupts();
if(1==TX_DONE)
{
IfxQspi_SpiMaster_isrTransmit(&g_spiMaster[1]);
}
else
{
}
}
void qspi1_Rx_ISR(void)
{
IfxCpu_enableInterrupts();
if(1==RX_DONE)
{
IfxQspi_SpiMaster_isrReceive(&g_spiMaster[1]);
}
else
{
}
}
And add TX,RX flag in transmit and receive code. but it doesn't works well. Still tx command is coming back to rx buffer.
i think even i set flag while i sending command by using enabled Transmit interrupt , disabled Receive interrupt, tx command is stored in rx buffer because of circut(MISO/MOSI is connected) and Rx buffer is storing it and return data when Rx interrupt called.
what should i modify more? please help me.
TX_DONE = 1;
RX_DONE = 0;
while (IfxQspi_SpiMaster_getStatus(&g_spiMasterChannel[1]) == SpiIf_Status_busy) {};
IfxQspi_SpiMaster_exchange(&g_spiMasterChannel[1], &g_tx_L_POS_u16[spi_num], &g_rx_L_POS_u16[spi_num][3], datalenth); //send command
// rx_QSPI1_Master();//set datapin as rx pin
// int data_num = g_tx_L_POS_u16[spi_num]&&0x000F; // get the number of data
TX_DONE = 0;
RX_DONE = 1;
for(int i=0; i<3;i++)
{
while (IfxQspi_SpiMaster_getStatus(&g_spiMasterChannel[1]) == SpiIf_Status_busy) {};
IfxQspi_SpiMaster_exchange(&g_spiMasterChannel[1], &g_tx_L_POS_u16[5], &g_rx_L_POS_u16[spi_num][i], datalenth);//g_tx_L_POS_u16[5] is 0x000u
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
https://github.com/Infineon/AURIX_code_examples/tree/master/code_examples/SPI_TLF_1_KIT_TC397_TFT
KIT_A2G_TC397_5V_TFT
For sch, please refer to above SPI part in the Triboard manual.
I suggest to study the TL35584 communication with TC397. Above materials are for your reference.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello. dw.
i read your links and solved my problem with refering below link.
my problem was 'chip select' signal was not keep low state while communication to pheriperal.
so i refered above linke and solved it.(set autoCS as '1', and set 'QSPI1_SSOC.B.OEN = 0' works.
but i have one more question.
i tried to set pin status with ' IfxPort_setPinState(&MODULE_P10, 0, IfxPort_State_low);' function.
but it doesn't works. so i used below code for directly access to register.
P10_IOCR0.B.PC0 = 0x10;
P10_OUT.B.P0 = 0;
why' 'IfxPort_setPinState()' function doesn't works?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi leekings, to avoid the interference by other part of code, please try to use a clean project to test P10.0.
Below GPIO code is helpful.