Apr 16, 2020
11:18 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Apr 16, 2020
11:18 AM
Hello Support,
In the AURIX 2G, there is a register SCU_STCON -- Start-up Configuration Register -- Offset 0xC4.
Bit 15 is STP.
Following sentences are in the User Manual Part 1 Revision 1.4 for STP bit
"
This bit will be always set by FW and can't be reset.
This bit is also cleared by an Application Reset.
STP is automatically set when a shutdown trap occurs.
"
1>
Looks like STP is cleared when Application Reset but during Cold Power On Reset it will be SET.
Is that correct?
2>
FW -- means Boot_ROM Firmware which is SSW
Is that correct?
3>
Can you please point me to documentation regarding "shutdown trap" as mentioned above?
Best Regards
In the AURIX 2G, there is a register SCU_STCON -- Start-up Configuration Register -- Offset 0xC4.
Bit 15 is STP.
Following sentences are in the User Manual Part 1 Revision 1.4 for STP bit
"
This bit will be always set by FW and can't be reset.
This bit is also cleared by an Application Reset.
STP is automatically set when a shutdown trap occurs.
"
1>
Looks like STP is cleared when Application Reset but during Cold Power On Reset it will be SET.
Is that correct?
2>
FW -- means Boot_ROM Firmware which is SSW
Is that correct?
3>
Can you please point me to documentation regarding "shutdown trap" as mentioned above?
Best Regards
- Tags:
- IFX
3 Replies
Apr 17, 2020
08:50 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Apr 17, 2020
08:50 AM
1> STP will be cleared on Application Reset therefore also on Cold Power On Reset (Application Reset is a "part" Cold Power On Reset)
2> Yes, FW means the SSW
3> Please see chapter 9.1.3.2 Shutdown and Reset Delay Timeout Counter (TOUTCNT) in the UM V1.4 part 1
2> Yes, FW means the SSW
3> Please see chapter 9.1.3.2 Shutdown and Reset Delay Timeout Counter (TOUTCNT) in the UM V1.4 part 1
Nov 10, 2022
07:48 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Nov 10, 2022
07:48 AM
I totally understand the description for the bit.
But the register STCON has access mode as ST, P0. P0 means a master can access it .
When I try to write 0 to this bit , I get SPB bus error meaning the master cannot access it. The access enable bit for the master is Enabled. Why is then the access mode P0 given ? Is it possible to modify the value to 0 at any point ?
Nov 10, 2022
12:26 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Nov 10, 2022
12:26 PM
Answered elsewhere - please just post questions in one spot 🙂
This widget could not be displayed.