Sep 09, 2021
08:43 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Sep 09, 2021
08:43 AM
Hello
I have following setup: Aurix + TLF35584.
I have following scenario:
During normal operation I set the PCSR of 33_2 to SCR, the SCR code sets the port to input, and cycic read the input in order to set the WAK pin of the TLF.
I can see that the SCR read ok the input as I watch in the debugger a variable that is set by SCR when the input goes High(also the WAK pin is set).
The issue:
- input is low, WAK is low, the Aurix commands the TLF to go to shutdown state, I have a trigger with an osciloscope on P33_2 to check if it goes to high.
- after the TLF gets the shutdown commands, somehow the 33_2_IN goes high, but I can not see anything on the osciloscope, so no external trigger.
Does it somehow, when Aurix is shut down the 33_2_IN goes by default to 1? I can say for sure that the WAK is trigger by the SCR(due to variables).
Thanks!!!
I have following setup: Aurix + TLF35584.
I have following scenario:
During normal operation I set the PCSR of 33_2 to SCR, the SCR code sets the port to input, and cycic read the input in order to set the WAK pin of the TLF.
I can see that the SCR read ok the input as I watch in the debugger a variable that is set by SCR when the input goes High(also the WAK pin is set).
The issue:
- input is low, WAK is low, the Aurix commands the TLF to go to shutdown state, I have a trigger with an osciloscope on P33_2 to check if it goes to high.
- after the TLF gets the shutdown commands, somehow the 33_2_IN goes high, but I can not see anything on the osciloscope, so no external trigger.
Does it somehow, when Aurix is shut down the 33_2_IN goes by default to 1? I can say for sure that the WAK is trigger by the SCR(due to variables).
Thanks!!!
- Tags:
- IFX
1 Reply
Jun 01, 2022
09:37 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jun 01, 2022
09:37 PM
Hello
Is "cycic" a typo?
Is AURIX TC3xx? Or is it TC2xx?
Best Regards,
Seiwa
This widget could not be displayed.