May 19, 2020
12:37 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
May 19, 2020
12:37 PM
Hello Support,
Can you please tell me under what condition RSTSTAT.SMU Bit 3 will be SET?
Can you please tell me under what condition TRAPSTAT.SMUT Bit 4 will be SET?
Will they both be SET together when SMU Alarm Configuration is either NMI [0x5] or RESET [0x6] or Interrupt [0x2, 0x3, 0x4]?
Will any of the above two bits will be set when all SMU Alarm Configurations are 0x0 or 01 [Inactive or Idle]?
May be you can provide me a decision table for conditions under which above two bits will be SET.

Best Regards
Can you please tell me under what condition RSTSTAT.SMU Bit 3 will be SET?
Can you please tell me under what condition TRAPSTAT.SMUT Bit 4 will be SET?
Will they both be SET together when SMU Alarm Configuration is either NMI [0x5] or RESET [0x6] or Interrupt [0x2, 0x3, 0x4]?
Will any of the above two bits will be set when all SMU Alarm Configurations are 0x0 or 01 [Inactive or Idle]?
May be you can provide me a decision table for conditions under which above two bits will be SET.
Best Regards
- Tags:
- IFX
0 Replies
This widget could not be displayed.