Apr 18, 2020
10:32 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Apr 18, 2020
10:32 AM
Hello Support,
For DISS bit in MTU_CLC Register of Aurix 2G, I find the following senetence :
"If the RMC field is implemented and if it is 0, DISS is set automatically"
1> What does "RMC" means?
2> For Aurix 2G, if MTU_CLC is now zero and I try to disable by writing MTU_CLC=1 [DISR=1], then after some time will be MTU_CLC.DISS=1 as the expected value.
Is that correct assumption?
Best Regards
For DISS bit in MTU_CLC Register of Aurix 2G, I find the following senetence :
"If the RMC field is implemented and if it is 0, DISS is set automatically"
1> What does "RMC" means?
2> For Aurix 2G, if MTU_CLC is now zero and I try to disable by writing MTU_CLC=1 [DISR=1], then after some time will be MTU_CLC.DISS=1 as the expected value.
Is that correct assumption?
Best Regards
- Tags:
- IFX
1 Reply
Apr 18, 2020
12:57 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Apr 18, 2020
12:57 PM
"RMC" stands for Run Mode Clock.
If a module is not used at all by an application, it can be completely shut off by setting bit DISR in its CLC register.
For peripheral modules with a run mode clock divider field RMC, a second option to completely switch off the module is to set bit field RMC to 00H.This also disables the module’s operation.
If a module is not used at all by an application, it can be completely shut off by setting bit DISR in its CLC register.
For peripheral modules with a run mode clock divider field RMC, a second option to completely switch off the module is to set bit field RMC to 00H.This also disables the module’s operation.