Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

nsyed
Level 5
Level 5
50 sign-ins First solution authored 25 sign-ins
Can you please clarify below questions related to the Clock Safety measures for AURIX TC3xx device

Does lock monitoring of fPLLx, fSPB detects only loss of clock failure mode ? or does it also detects clock above/below the nominal frequency.

For example if my fPLLx is configured for 300Mhz and during runtime fPLLx frequency reduces to 270Mhz (10% less than actual value) will the Clock monitoring be able to detect it ?

From the reference manual looks like, it cannot ? Can you please confirm my understanding
1 Reply
NeMa_4793301
Level 6
Level 6
10 likes received 10 solutions authored 5 solutions authored
See also 4.2.7.2 CLOCK in the Safety Manual. The Oscillator Monitor will detect a stopped oscillator, or an oscillator running at an incorrect harmonic. The PLL will only signal an alarm on loss of lock.

So, no, it won't detect a 10% difference - but ESM[SW]:CLOCK:PLAUSIBILITY can, depending on the implementation.
0 Likes