Question on TC3xx - ESM[HW]:SYS:SW_ERROR_PIN_MONITOR

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
nsyed
Level 5
Level 5
5 likes given 100 sign-ins 50 sign-ins

Hello,
TC3xx - ESM[HW]:SYS:SW_ERROR_PIN_MONITOR indicates that the

A component independent from the AURIX microcontroller shall monitor the SW based External Failure Reporting Interface. The SW-based External Failure Reporting Interface provides a fast information about the presence of an internal failure of the microcontroller.

Can you please clarify what are the SW based External Failure Reporting Interfaces ?
Can you please give one example to help better understand this requirement ? I am having hard time trying to understand which interfaces should be used to satisfy this requirement.

0 Likes
1 Reply
Aiswarya_A
Moderator
Moderator
Moderator
25 likes received 250 sign-ins 50 solutions authored

Hi, 

This cannot be discussed under public forum since this topic is covered under NDA.

Regards,
Aiswarya.

0 Likes