Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

nsyed
Level 5
First solution authored 25 sign-ins 100 replies posted
Level 5
Hello,

Can I configure Application/System Reset to re-initialize/clear DSPRs/PSPRs ?

I have selected following configuration, however DSPRs/PSPRs are not getting cleared when I command application reset via using IfxScuRcu_performReset iLLD API.
- DMU_HF_PROCONRAM.RAMIN = 0 (Init_All, RAM initialization is performed after cold power-on- reset and warm power-on-reset.)
- DMU_HF_PROCONRAM.RAMINSEL = 0 (RAMs (PSPR, DSPR, PCACHE and DCACHE) in CPU0, CPU1 & CPU2 are selected for initialization)

Any thoughts ?
0 Likes
1 Solution
NeMa_4793301
Level 6
10 solutions authored 5 solutions authored First solution authored
Level 6
PROCONRAM only applies to cold power on reset (power restored) or warm power on reset (PORST asserted).

If you want to initialize RAM after an application or system reset, using the Memory Test Unit is the fastest way.

View solution in original post

0 Likes
1 Reply
NeMa_4793301
Level 6
10 solutions authored 5 solutions authored First solution authored
Level 6
PROCONRAM only applies to cold power on reset (power restored) or warm power on reset (PORST asserted).

If you want to initialize RAM after an application or system reset, using the Memory Test Unit is the fastest way.
0 Likes