Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

leonng
Level 3
Level 3
First like given 10 questions asked 10 replies posted

Hi there,

 I want to ask how to set the Tx is low when it isn't in active. TC234 is used.

The output:

WhatsApp Image 2023-02-03 at 09.57.05.jpeg

The goal:

WhatsApp Image 2023-02-03 at 09.57.03.jpeg

Thank you!

Best Regards,

Leon

0 Likes
1 Solution
cwunder
Employee
Employee
50 solutions authored 250 sign-ins 25 likes received

As far as I remember the MTSR pin will continue to output the last bit value sent from the shift register. If your last bit of data that is being transmitted is a '1' then the output will remain high after the frame has finished. If you want the output to be low then you could send a dummy transfer (without a real chip select to an actual device) with the data set to zero to clear the output pin. 

View solution in original post

1 Reply
cwunder
Employee
Employee
50 solutions authored 250 sign-ins 25 likes received

As far as I remember the MTSR pin will continue to output the last bit value sent from the shift register. If your last bit of data that is being transmitted is a '1' then the output will remain high after the frame has finished. If you want the output to be low then you could send a dummy transfer (without a real chip select to an actual device) with the data set to zero to clear the output pin. 

This widget could not be displayed.