Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

User22868
Level 2
5 questions asked 10 replies posted 25 sign-ins
Level 2

I am working on QSPI using TC367 Micro. QSPI is configured as Master in Long Mode with a frame length of 16bytes (4 words, same as max FIFO size) and I am using DMA (Qspi in Single Move Mode) to move the data from RXEXIT to a RAM buffer.

My Slave is another TC367 Micro. 

When communication with slave is working fine, if I turn off Power to Slave controller, I am expecting RXEXIT in Master shall receive all FF as data or partial FF depending on when the power to Slave controller is turned off. 

But, when I am checking my Rx RAM buffer in Master (that holds the data from RXEXIT via DMA), the data sometimes come out all zeros (0x00000000) for 3~4 times and then changing to all FF's (0xFFFFFFFF).

I am thinking to use the concept that if my Rx RAM buffer value in Master is all FF, then consider this as SLAVE timeout. But, due to the above mentioned issue for 3~4 times of zeros, I am not able to use this concept.

Any thoughts of why RXEXIT might be updated to zero's first and then 0xFF's?  or is there any other way to detect SLAVE is timed out?

Thank You

0 Likes
3 Replies
Prudhvi
Moderator
Moderator 25 solutions authored 10 likes received 100 sign-ins
Moderator

Hi,

I'm not sure if the idea to check the SLAVE_TIMEOUT based on the data is okay, let me check internally and will update you. Is your implementation idea based on the below statement ? 

                                                   Prudhvi_0-1659105854260.png

There could be corner case scenario in the run-time may be an Underflow event occurs but still SLAVE is working properly. In this case the Master assumes Slave is timed-out but may not be in real but I'll update you on this.

Regards,

Prudhvi.

 

Regards,

Prudhvi.

User22868
Level 2
5 questions asked 10 replies posted 25 sign-ins
Level 2

@Prudhvi Thank you for the feedback. I agree with you. Relying on Rx data values is not a great way for detecting Slave Timeout. Thanks again for checking on this, any ideas would be a great help!

0 Likes
User22868
Level 2
5 questions asked 10 replies posted 25 sign-ins
Level 2

@Prudhvi Just checking if you or anyone have had a chance to think about the possible ways to detect SLAVE MIA..

0 Likes