Announcements

Equip yourself to optimize AURIX™ MCUs for Evs at the EV Webinar. Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

User17382
Level 1
Level 1
Hi,
I cannot connect to my application board (the one with TFT display) via USB. I have installed the Hightec Free Entry tool chain and my board is connected via Micro-USB cable directly to my PC. I want to debug with UDE, but there is no device found when using UDE.**
BR Cosmo

#8042000 12393
0 Likes
1 Reply
User17279
Level 1
Level 1
Hi,
Have you installed the Device Access Server (DAS) from Infineon?**
DAS is needed to connect to Infineon's Application-Kit or TriBoard via USB. You can download it at www.infineon.com/das*
Once DAS is installed you can check for connected devices with the DAS Device Scanner.
Berl
0 Likes