Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

User17897
Level 2
Level 2
I test the performance difference between int and float through "dotp"(res += a*b).
I found the speed of int is slower than float, about half.
Why?I want to know.
6 Replies
User13290
Level 5
Level 5
First like received First solution authored

Hi Shaquille,

Can you list the sample code for the integer and float sample case? Just so that we get a better understanding of what you're doing.

Best regards,

Henk-Piet Glas

Principal Technical Specialist
Embedded Software

0 Likes
User17897
Level 2
Level 2
float test:
IfxCpu_resetAndStartCounters(IfxCpu_CounterMode_normal) ;
for(i = 0 ; i < iTryCnt ; i ++)
pDotpResF = Test_float_dotp(pAF, pBF, iDataCnt) ;
perfCounts = IfxCpu_stopCounters() ;

int test:
IfxCpu_resetAndStartCounters(IfxCpu_CounterMode_normal) ;
for(i = 0 ; i < iTryCnt ; i ++)
pDotpResI = Test_int_divp(pAI, pBI, iDataCnt) ;
perfCounts = IfxCpu_stopCounters() ;

implementation of Test_float_dotp:
float Test_float_dotp(const float* pVecA, const float* pVecB, int iDataCnt)
{
int i = 0 ;
float fResult = 0.0f ;
for(i = 0 ; i < iDataCnt ; i ++)
fResult += pVecA * pVecB ;

return fResult ;
}

implementation of Test_int_dotp
int Test_int_dotp(const int* pVecA, const int* pVecB, int iDataCnt)
{
int i = 0 ;
int iResult = 0 ;
for(i = 0 ; i < iDataCnt ; i ++)
iResult += pVecA * pVecB ;

return iResult ;
}

result is:
float dotp cost(64*64): 17689tick
int dotp cost(64*64): 34008tick


Is there something wrong in above code?
0 Likes
lock attach
Attachments are accessible only for community members.
User13290
Level 5
Level 5
First like received First solution authored

Hi Shaquille,

Code looks OK to me. I used the attached sample case, using parts of your code. To build it I used:


tricore-gcc -O2 -mcpu=tc39xx main.c dotint.c dotflt.c -o benchmark.elf


I then simulated it as below:


tsim16p_e -MConfig MConfig -disable-watchdog -H -g -s -x 0 -o benchmark.elf


Which then generates the following output:


Integers: 0x000000E9 cycles
Floats: 0x000000E8 cycles


So floats are still faster, as in your case, but only by 1 cycle. What command line options have you been using?

Best regards,

Henk-Piet Glas

Principal Technical Specialist
Embedded Software

0 Likes
User17897
Level 2
Level 2
sorry, I make a mistake again, divp instead of dotp for int-test:(
0 Likes
User13290
Level 5
Level 5
First like received First solution authored

Hi Shaquille,

No problem. If there's anything else I can help you with, just let me know.

Best regards,

Henk-Piet Glas

Principal Technical Specialist
Embedded Software

0 Likes
User18504
Level 3
Level 3
Hello,
I just posted a new topic with the same thematic.
Could you join it here?
Also is there some drawback in using floats for precision calculation instead of int?
As the performance is almost the same, probably by using directly float instead of some integer with LSB and offset, probably even more time could be spared.
Does the TC277 have a separate FPU that operates separately from the integer unit?
Can they operate in parallel also?
0 Likes