Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

User17740
Level 3
Level 3
First like received
Hi all,

Compared between TC213 and TC233, the Pin 48 in TC233 is Vdd and the Pin 48 in TC213 is NC (not connected). I am planning to use identical pin layout that means the Pin 48 (NC) in TC213 may be connected to Vdd. One app note says NC pins are recommended in general to be not connected. Is it possible to connect NC Pin 48 in TC213 to Vdd for this special case?

Thank you
B.

#8042000 12562
0 Likes
1 Reply
User17612
Level 3
Level 3
First like received
Hi,

it is acceptable to connect pin 48 to VDD on TC213. This is SCDCDC output on TC233, which is not available in TC213.

Best
Lucas
0 Likes