Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

prafull23
Level 1
Level 1
10 sign-ins 5 sign-ins First solution authored

Hi everyone,

 

I have MiniWiggler V3 and i have been trying to find proper documentation on how use this this debugger for flashing as well as debugging with Aurix Development Studio.
How i understood is that i need to start DAS device scanner. After that click on Start DAS Server. It will open DAS Server Control Panel.
I'm using DAP connection along with Aurix TC322 custom micro-controller.
I have selected Custom board while creating this project.
I have the following view.

 

prafull23_0-1678207128680.png


question 1: Why i do not have "show all target" option and see only Generic Infineon AURIX Board ?
question 2: Is the memtool used for flashing on the micro controller ? or is it also possible to flash from ADS?

Regards,

Prafull

0 Likes
2 Replies
Aiswarya
Moderator
Moderator
Moderator
50 replies posted 100 sign-ins 10 solutions authored

Hello,

1. Could you please clarify on this statement? Generic Infineon AURIX Board is the default option and you can select your specific device in configuration.

2. Yes. Memtool is used for flashing on the microcontroller. It is also possible to flash from ADS.

Regards,
Aiswarya.

0 Likes

1. I do not see any option as for Selecting specific device configure. could you walk through it ? or give detailed document for these steps ?

 

2. Thanks

 

Regards,
Prafull

0 Likes
This widget could not be displayed.