Jan 13, 2023
03:40 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jan 13, 2023
03:40 AM
Hello,
As per below max power pattern,
Can you pls confirm the current consumption (IDD) at VDD level = 1.375V will be as below for max pattern?
Also, its mentioned that sum of all currents = 597mA (for real power pattern) as below –
Does it includes all current at Vext = 5.5V, Vdd = 1.375V & Vddp3 = 3.63V ?
Can you pls let us know what is the “Sum of all currents @ for max power pattern” ?
In brief (as per datasheet) –
At Vext = 5.5V, max power pattern current consumption will be 44 mA,
At Vdd = 1.375V, max power pattern current consumption will be 650 mA,
At Vddp3 = 3.63V, max power pattern current consumption will be 45 mA.
Regards,
Abhishek D.
0 Replies