Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
MathewCrawford
Level 1
Level 1
First reply posted First question asked Welcome!

I am experiencing a problem with Enabling the SSH for one of our SRAM. We are working with the Tricore TC334LP, and trying to enable the SSH (ultimately to run SRAM Init) for DMEM, PMEM, AND DMEM1. The processing that we are using appears to work correctly for both DMEM and DMEM1, but the same processing for PMEM results in some kind of lock-up. I can step thru with a (Lauterbach) debugger successfully, but when free-running it gets hung up in the wait loop immediately after enabling the PMEM SSH, using either:

MTU_MEMTEST0.B.CPU0_PMEM_EN = 1U;
or:
MTU_MEMTEST0.U |= 0x00000004U;

Prior to this enable, we are jumping to the init routine with a link (rather than function call), disabling PCACHE (as well as DCACHE - in case it might have been enabled in boot), enabling the MTU, disabling the write-protection for registers (SAFETY ENDINIT), and disabling Error Reporting to the SMU for the SSH (MISCE and OPENE). As I have said, this logic seems to work fine for DMEM and/or DMEM1, but the same logic does not work for PMEM SSH enable.

0 Likes
3 Replies
DownyK
Level 5
Level 5
100 replies posted 10 solutions authored 250 sign-ins

Hi, Mathew Crawford

when you test PMEM, which core do you use?

The core should not check its own SRAMS because of Stack usage. 

Therefore I recommend Core1 checks Core0 located RAMs and vice versa.

0 Likes

Unfortunately, we are single-core, so we are trying to implement this with no stack nor RAM variable access.

0 Likes
Yuva
Moderator
Moderator
Moderator
250 replies posted 250 sign-ins 100 solutions authored

Hello,

Please update the following details

1. Does it continue after some time or is it stuck forever?
2. What content is put in PSPR memory with the linker script?
3. Is there a possibility for any interrupts to happen?
4. Are there chances for other masters to access PMEM?

Thanks.

0 Likes