Not applicable
Aug 14, 2014
09:23 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Aug 14, 2014
09:23 AM
Hi,
In the MPU implementation, DPR0_L & DPR0_U are 32 bit aligned registers. For DPR0_L, the key word “align in the linker will ensure the alignment, however for DPR0_U this is not guaranteed. If the DPR0_U is not 32-bit aligned, while writing into the register, the address is truncated to the lesser nearest 32-bit address. Thus how can an application ensure that the MPU registers are not loaded with the truncated ranges, because at runtime, if a variable that exist into the truncated region is accessed, a fault will be encountered.
E.g. For a memory section in range 0x70000028 and 0x70000034 for this the DPR0_U will be truncated to 0x70000030, thus any access to variables in range 0x70000030 and 0x70000034, will cause a fault, which is undesirable.
I am reading the memory section in linker as -
"START_APP1_BLOCK0" := addressof(group:APP1_BLOCK0);
"END_APP1_BLOCK0" := addressof(group:APP1_BLOCK0) + sizeof(group:APP1_BLOCK0);
Platform used - Tasking 4.2r2
In the MPU implementation, DPR0_L & DPR0_U are 32 bit aligned registers. For DPR0_L, the key word “align in the linker will ensure the alignment, however for DPR0_U this is not guaranteed. If the DPR0_U is not 32-bit aligned, while writing into the register, the address is truncated to the lesser nearest 32-bit address. Thus how can an application ensure that the MPU registers are not loaded with the truncated ranges, because at runtime, if a variable that exist into the truncated region is accessed, a fault will be encountered.
E.g. For a memory section in range 0x70000028 and 0x70000034 for this the DPR0_U will be truncated to 0x70000030, thus any access to variables in range 0x70000030 and 0x70000034, will cause a fault, which is undesirable.
I am reading the memory section in linker as -
"START_APP1_BLOCK0" := addressof(group:APP1_BLOCK0);
"END_APP1_BLOCK0" := addressof(group:APP1_BLOCK0) + sizeof(group:APP1_BLOCK0);
Platform used - Tasking 4.2r2
- Tags:
- IFX
2 Replies
Aug 18, 2014
12:11 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Aug 18, 2014
12:11 PM
amitoza88 wrote:The protection registers require 64-bit (8 byte) alignment, since the lower 3 bits are always 0.
In the MPU implementation, DPR0_L & DPR0_U are 32 bit aligned registers. For DPR0_L, the key word “align in the linker will ensure the alignment, however for DPR0_U this is not guaranteed. If the DPR0_U is not 32-bit aligned, while writing into the register, the address is truncated to the lesser nearest 32-bit address. Thus how can an application ensure that the MPU registers are not loaded with the truncated ranges, because at runtime, if a variable that exist into the truncated region is accessed, a fault will be encountered.
E.g. For a memory section in range 0x70000028 and 0x70000034 for this the DPR0_U will be truncated to 0x70000030, thus any access to variables in range 0x70000030 and 0x70000034, will cause a fault, which is undesirable.
I am reading the memory section in linker as -
"START_APP1_BLOCK0" := addressof(group:APP1_BLOCK0);
"END_APP1_BLOCK0" := addressof(group:APP1_BLOCK0) + sizeof(group:APP1_BLOCK0);
Platform used - Tasking 4.2r2
I'm not sure how you're defining the APP1_BLOCK0 group, but if you can make it 8 bytes bigger, and make sure subsequent sections are also aligned to an 8-byte boundary, then the alignment of DPR0_U will always be okay. It might be as easy as this:
"END_APP1_BLOCK0" := addressof(group:APP1_BLOCK0) + sizeof(group:APP1_BLOCK0) + 8;
Not applicable
Aug 18, 2014
12:19 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Aug 18, 2014
12:19 PM
Hi Neal,
Thanks for the clarification. However do we have any application note or this documented in any Infineon documents? I will need to refer that in my design document.
If you are aware about any such reference, kindly share.
Thanks for the clarification. However do we have any application note or this documented in any Infineon documents? I will need to refer that in my design document.
If you are aware about any such reference, kindly share.