Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

AURIX™ Forum Discussions

Not applicable
Hi,

I have purchased KIT_AURIX_TC297_TFT. I have LCDDemo_Appkit-TC297TFT project (availble in HighTech Examples) into the board.
After that the board is continuously resetting and when I try to flash another program into it, it is not being detected in the HighTech Development Platform Runtime. It says Core0 not connected.
How can I come out of this set?

Also, is there any User manual for this Starter kit?

Quick response will be appreciated.

Thanks,
Divya
0 Likes
1 Reply
cwunder
Employee
Employee
50 solutions authored 250 sign-ins 25 likes received
For the starter kit user manual you need to request access on the myInfineon site. see post https://www.infineonforums.com/threads/4716-Trying-to-find-manual-of-TC277-for-ethernet-Where-is-it

Concerning the problem to connect to the Starter kit perhaps the watchdog functionality of the TLF35584 is causing a problem. Note you should not see a continuous reset, you should only see it twice then stop until you active the wake button again (or power it again).



See this post for more information on how to solve it https://www.infineonforums.com/threads/4219-Application-Kit-TC2X7-Flashing-not-possible-after-testin... and https://www.infineonforums.com/archive/index.php/t-4219.html?
0 Likes